Question: External loop compensation of MAX17502. The value of RZ calculated for the design in figure 9 of the datasheet comes out to 36kohm (6000 x 50000 x 10uF x 12V). But in the datasheet RZ=20kohm…
Yes in the configuration given in App Note 5775 the EN/UVLO voltages are still 1.218V (nominal) to enable, and 1.135V (nominal) to disable. However, the manner in which the circuit is set up in this configuration…