Article Does the Enable Transient Protection feature on the MAX17223 incur additional current draw when EN is connected?

The MAX17220, MAX17222,and MAX17224 have the Enable Transient Protection feature and will require a high impedance pull up  (application dependent, typically 33
Meg)  on the EN pin which adds around 61nA ​to the quiescent current with VIN=1.5V, VOUT=3.3V and efficiency=85%.

The MAX17221, MAX17223, and MAX17225 do not have the Enable Transient Protection and the EN pin can be tied to the input voltage without any extra current draw.