Q: What is the function of the INX pin on the MAX15108A? Should it be shorted to IN, as in the typical application schematic, or should it be low-pass filtered, as in the EVKIT?
A: IN is the input for…
Answer: Several solutions exist: DDR4 operates at a voltage between 1.2 V and 1.4 V with a frequency between 800MHz and 2133 MHz. The MAX1510/MAX17510 DDR linear regulators source and sink up to 3A peak…