MAX15096AGWE+T: FAQ

  • Created
Was this helpful?
  • Is there a way to disable the UVOV feature on the MAX15096?

    Yes - the UVOV feature can technically be disabled by clamping the voltage on this pin using a voltage inside the window. The zener voltage will have to be turned on for the minimum input voltage that…
  • MAX15096 Hot-Swap PG glitch issue

    Q: When we make OUT pin(12V) of MAX15096GWE+T into short by using load machine, glitch will occur in PG pin. Based on spec, the behavior is not reasonable. Could you help to confirm the issue? …
  • MAX15096 OCP formula at low Vin application

    Q: In application, MAX15096 OCP is set to 0.5A (Rcb = 5.49kohm) and Vin is 3.3V. The test result shows the OCP point has >10% tolerance. We don’t specify the tolerance in DS at that low current. Do you…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.