Maxim does not recommend nor have we tested under load current conditions of greater than 8A. However the load current only concerns the external FETs. In theory if the external FETs are rated sufficiently…
The MAX15068 has internal clamp range for IPMON pin's voltage, typical value is 2.3V.
If customer wants to send this value to SOC, they should double check the SOC's IO pin input range,
If less than…