Article Does the MAX15062 employ current sense blanking during the FET switching transitions?

Does the MAX15062 employ current sense blanking during the FET switching transitions?

 

Yes all our DC-DC converters we make are designed with internal current sense blanking.

This current sense blanking time is  the main component of the “minimum ON time” specification in the datasheet and is the sum of blanking time plus other delays in the circuit.

For the MAX15062, minimum on-time is specified to be 90ns nominal, with a maximum of 130ns.