Article What is the reason of the MAX15021 output voltage overshoot at start-up in EESim?

We confirmed the EESim model has two problems (not found in the silicon):

  1. Soft start is not working correctly (Vout should ramp up over several hundred milliseconds, at least)
  2. Low output voltages do not regulate correctly with 5V input (but seem to regulate OK with 3.3V input)

We are working on the issue to fix it, although there is no date in sight.