Article Can I use LTC4418 for Higher Current Application up to 60A?

Answer:

Though the typical application sample circuits in the datasheet are for low output currents (<2A), the LTC4418 can also be used at higher loads if the external MOSFETs are appropriately selected. The maximum continuous load current is limited by the external MOSFETs for the PowerPath applications.

Another thing to note is that the LTC4418 is designed to work with P FETs which typically have a more limited current handling capability when compared to a similarly sized N FET. P FETs typically have a larger Rdson so will experience higher conduction losses.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.