Article How is voltage noise of an LDO measured?

Q.

How is voltage noise of a LDO measured?

-------------------------------------------------------------------------------

A.

LDO noise is measured two ways 1) Total RMS noise over a specified bandwidth, and 2) Noise spectral density at several frequencies over a specified range.  To measure the RMS noise, the noise of the LDO is amplified with a low noise preamp before being measured with a true RMS voltmeter.  The preamp bandwidth is 10Hz to100kHz, and is set by fourth order filters.  The preamp gain is 60dB with a noise floor of less than 1uVrms referred to the input. The noise spectral density measurements are made with a lock-in amplifier with a 1Hz bandwidth.  This is essentially a narrowband receiver that can be tuned over a wide range of frequencies.  The noise spectral density per root Hertz is measured with a voltmeter and a plot of the Noise Spectral Density vs Frequency is generated.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.