Article What is the current capability for the PWM output pins of the MAX31785?

The source/sink capability of the PWM output is in the VOH1 and VOL1 specifications.  The PWM output pins can sink 4mA and source 2mA.