Question The ADP2504 not achieving the max 1 amp as defined in the spec. Answer The ADP2504 is designed to start-up with a maximum of 100uF, if you have
additional capacitance besides the 22uF shown…
Q
The ADP2504 not achieving the max 1 amp as defined in the spec.
A
The ADP2504 is designed to start-up with a maximum of 100uF, if you have additional capacitance besides the 22uF shown on the…
Question The ADP2504 does not seems to provide the requested voltage (5V) WHEN A SLOW RISING Input is applied (bench power supply) at power up.Looks like the adp2504 is timing out and locking at the same…