ADP198: FAQ

FAQ

  • Created
  • Updated
Was this helpful?
  • ADP198 What happens when Vout > Vin ?

    Question What happens with Vin , when Vout is greater than Vin ? Answer The valid input range really only applies to normal operation, of course the input voltage can fall below 1.65V but them the device…
  • ADP198  What happens when Vout > Vin ?

    Q What happens with Vin , when Vout is greater than Vin ? A The valid input range really only applies to normal operation, of course the input voltage can fall below 1.65V but them the device will…