ADP1607: FAQ

  • Created
  • Updated
Was this helpful?
  • ADP1607 to supply ADAU1761

    Question I'd like to use the ADP1607 to supplying the ADAU1761 for a mobile audio project (single cell). For suppling by USB or external supply I inteded a LDO. To avoid voltage drop I shoudn't use…
  • ADP160-IGND Max

    Question In the ADP160/ADP161/ADP162/ADP163 datasheet, table 1 states IGND maximum @ Iout=10mA is 19uA, but in the figure 16 IGND @ Iout=10mA can be 100uA (when Vin is 3.3v). Can you clarify?…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.