Article Voltage Regulator for 16-bit ADC AD7626

Question

We are looking for an appropriate low-noise, low-drop voltage regulator to
power the 16-bit ADC AD7626. Which device is a better fit : ADP3334 (5V, 2.5V)
or ADP7104 (5V, 2.5V)? Is there any other voltage regulator that is more
suitable than those both devices?

Answer

For the 2.5V rails I suggest that you use the ADP151 low noise LDO for the
lowest noise solution. For a lower dropout voltage the ADP124/125 will work at
the expense of higher output noise. If two 2.5Vout LDOs are needed (VDD2 & VIO)
we have the dual output ADP223.

For the 5V rail you will need the higher Vin ADP7102 or ADP7104, they have
fixed 5Vout options. This assumes power source greater than 5.5V.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.