ADM2682E: FAQ

FAQ

  • Created
  • Updated
Was this helpful?
  • ADM2682E start up currents

    Hi. What is the expected value of ADM2682E start up current when driving 120R load and no load conditions. We encountered with an interesting situation. We have 5V/250mA power supply and our circuit…
  • ADM2682E/ADM2687E Creepage and Clearance

    Q What creepage and clearance does the ADM2682E/87E have, and what do these characteristics refer to? A The ADM2682E/87E has more than 8 mm of creepage and clearance. Creepage refers to the shortest…
  • ADM2682E/ADM2687E Isolation Voltage

    Q What isolation voltage does the ADM2682E/87E meet? A The ADM2682E/87E provides an isolation withstand voltage of 5 kVrms per UL1577 between the two sides of the isolation barrier. This is the…
  • ADM2682E/ADM2687E providing additional current to external devices

    Q Can the internal isolated DC/DC converter provide additional current to external devices using the Visoout pin? A No, the internal DC/DC converter only has sufficient power to power the RS-485…
  • ADM2682E/ADM2687E Recommended Application Notes

    Q Do you have any recommended application notes that would help design in the parts? A Please go to www.analog.com and search for: AN-0971: Recommendations for Control of Radiated Emissions with…
  • Difference between ADM2682E and ADM2687E

    Q What are the differences between the ADM2682E and ADM2687E? A The only difference between the two parts is the data-rate, the ADM2682E is a 16Mbps part and the ADM2687E is a 500kbps part.
  • Key difference between the ADM268xE and ADM258xE

    Q What’s the key difference between the ADM268xE and ADM258xE? A The key difference is the isolation rating. The ADM268xE is a 5kVrms rating per UL1577, whereas the ADM258xE is a 2.5kVrms per UL1577…