ADM1066: FAQ

FAQ

  • Created
  • Updated
Was this helpful?
  • ADM1066 AUX Signals in the State Machine

    Question How can I use the AUX signals in the ADM1066 power on state machine? Wewant to use the AUX signals as power down and device insertion protect. Answer The AUX signals are monitored using the ADC…
  • ADM1066: application questions

    Question 1. In the closed-loop margining application as showed in Figure 33 in datasheet, if DACOUTn is placed with midcode at 1.0V, DC/DC output (VPn) is supposed to be 3.4V as normal voltage, and…
  • DAC power up default state of ADM1066

    Q For ADM1066, after power on, what's the DAC's output? 0V or mid-scale value? I read the datasheet and it says DAC pin is high impedance, I am not sure what that means for DAC output? I hope you can…