Article Why does the LT8304-1 sometimes restart the soft-start cycle multiple times during power-up?

During the LT8304-1’s internal 11 ms soft-start period, the controller checks whether the voltage across the external ground-referred reference resistor (RREF) exceeds a threshold—typically 0.6 V, which corresponds to approximately 60% of the target output voltage. If this condition is not met by the end of the soft-start timer, the device automatically initiates a new soft-start cycle.

This behavior is expected under certain conditions, such as:

  • Output short circuits, where the voltage cannot rise due to a fault.
  • Excessive output capacitance, which can delay the voltage ramp-up, preventing the threshold from being reached in time.

As a result, the LT8304-1 may perform multiple soft-start attempts until the output voltage reaches the required level.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.