Article How is the VOUT feedback signal interfaced to the PWM logic in the MAX20029?

The MAX20029 is a peak current mode control device. The OUTS pin is the feedback pin that feeds into comparator against Vref. It connects the feedback select block, which is a network of resistor dividers to set the output voltage. If there is a feed forward capacitor, it is only there to improve phase margin and bandwidth with the additional pole and zero.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.