Article How to select current limit in MAX17250 design?

The MAX17250 has a three-state ISET input pin used to select the inductor peak current limit (IPEAK), as shown in the Table.

ISET       IPEAK (A) 

VL           3.5
AGND     2.7
OPEN     1.85

ISET value is read when VL crosses its UVLO threshold during power-up, or when EN transitions low-to-high. (See VL UVLO in the Electrical Characteristics table).

The inductor peak current limit setting should be determined as follows:
1. Calculate the inductor ripple current (ΔI) using the equation below.

ΔI=VIN_MIN×tONL, where VIN_MIN is the minimum input voltage, tON is the 800ns on time.

2. Calculate the maximum input current (IINPEAK) using the equation below:

IINPEAK=VOUT×IOUTVINMIN×η+ΔI

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.