Article Why does the MAX15303EVKIT use a 1k ohm resistor on the INSNS and LXSNS pins? (while the datasheet recommends using 2k ohm)

Both pins have an internal voltage divider to step down the input volage and LX voltage to inputs of comparators. The total impedance of voltage divider is larger than 200Kohm so using 1K or 2K at INSNS and LXSNS pin won’t impact the behavior of the device. The EVKIT board has been road tested so it is recommended to follow the EVKIT design.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.