Post Go back to editing

Provision for Warm boot in Bytepipe_HDK Rflan

Category: Software
Product Number: ADRV9002
Software Version: TES 0.25.0 , Bytepipe_Rflan v12.08.22

Hello,

We are trying out some narrowband features of the PFIR in the ADRV9002 using Bytepipe_HDK (rflan) platform. The ADRV9002 documentation limits us to use a filter bandwidth not less than the carrier bandwidth divided by a factor of five (Ref1) to avoid any calibration errors. However, the ADRV9002 user guide (Ref 2) suggests bypassing the calibration procedures (probably via  warm boot). Does the Bytepipe_HDK_rflan provide any warm boot features / is there any source code which enables/disables or calls warm boot via ADRV9002 warm boot APIs? 

[Warm boot viaTES GUI and profile creation/loading of the same does not seem to be an option as warm boot is not supported via TES (Ref3)]. ADRV9002 forums suggest the API method and provide an example code with minor modifications in the "main.c" file that is generated from TES GUI Sample code (profile making). This "main.c" however seems to be obsolete wrt Bytepipe_HDK (rflan) as the "rflan.c" & "adrv9001.c" files contain the main routines. 

Any help regarding warm boot provisions/options in Bytepipe_HDK (rflan) and/or narrowband PFIR loading (without initialization and calibration errors) would be appreciated.

Thanks!

Ref 1:


Ref 2:

Ref 3:
Using Warmboot Via API - Documents - TES GUI & Software Support ADRV9001 – ADRV9007 - EngineerZone (analog.com)