Post Go back to editing

HDL Driver support & Validation status with LSSI 1- lane with serialization factor of 32 & LSSI 2- lane with serialization factor of 16

Category: Hardware
Product Number: BP-3EG1E-9002

Hello,

We are exploring  BP-3CG1E-9002 & BP-3EG1E-9002 for our internal development perspective. 

We need to get complete 16 bit I &16-bit Q samples from ADRV9002. So, we want to configure the ADRV in modes as mentioned below (any one)

  1. LSSI 1- lane with serialization factor of 32
  2. LSSI 2- lane with serialization factor of 16

Mainly, we do not want the limitation to use Serialization factor of 12 in LSSI- 2 lane mode.

Can anybody please confirm that the SOM & the HDL baseline (& ADRV9002 driver) supports above mentioned configuration without any limitation?  

UG-1828 (Rev. 0) (analog.com) -  Page 59

With Regards,

Hariprasad Bhat