Hello,
I wanted to ask, is there a general application you can provide to get up and running controlling it without having to write all our custom code?
Thank you.
Hello,
I wanted to ask, is there a general application you can provide to get up and running controlling it without having to write all our custom code?
Thank you.
Is this related to RadioThorium?
Assuming this is regarding RadioThorium, the default power up state for the SC2444 is the same as the example provided in the API Spec (attached) in section 5.1.1, in brief:
IF and FDD modes enabled
2.345 GHz IF on both Tx and Rx Paths
PDFRF output of 26.985 on Tx
Yes. Sorry about the delay.