Post Go back to editing

Radio Thorium

Hello,

On the Radio Thorium 24 - 44 GHz Module, I noticed that the switchable bandpass filter seemed to not be tunable (move the center frequency).  I wanted to verify with you if that is true?

Is it an analog part that you can share with me?  Or are they some switches and filters chosen by your team?

Thank you. 

  • The switchable bandpass filter is made up of switching fixed filters into the signal chain.  The bandwidth and the center frequency of the filters are listed below.

    20 MHz BW centered at 2017.5 MHz
    50 MHz BW centered at 2345 MHz
    100 MHz BW centered at 2350 MHz
    200 MHz BW centered at 2593 MHz
    400 MHz BW centered at 2300 MHz
    800 MHz BW centered at 2400 MHz
    1400 MHz BW centered at 2500 MHz
    Bypass path, no filtering