Hello,
Currently I use an emStat pico module interfacing stm32f4 microcontroller. Initially, I tested to get firmware version of the module, then I get it correctly. Here is the initial results:
EMSTAT_PICO Firmware Version: tespico1304#Oct 22 2021 14:3EMSTAT_PICO Firmware Version: tespico1304#Oct 22 2021 14:38:26 R*
Then I try to send the MethodScript, I get "e!0009: Line 1, Col ", '\0' <repeats 29 times>" error. Do you have any suggestion to solve the problem? Here is my code:
uint8_t firmware_version_response[36]; uint8_t response_buffer[50]; uint8_t firmware[2] = "t\n"; int isConnected = 0; const char * dummy = "fs_dir /measurements\n"; void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { HAL_UART_Receive_IT(&huart3, response_buffer, 5); } int main(void) { HAL_Init(); SystemClock_Config(); MX_USART2_UART_Init(); MX_USART3_UART_Init(); /* USER CODE BEGIN 2 */ HAL_UART_Receive_IT(&huart3, firmware_version_response, 36); HAL_UART_Transmit(&huart3, firmware, 2, 0xffff); while (1) { if(isConnected == 0) { if(strstr(firmware_version_response, "espico") != NULL) { uint8_t fresponse[] = "EMSTAT_PICO Firmware Version: "; HAL_UART_Transmit(&huart2, fresponse, sizeof(fresponse), 0xffff); HAL_UART_Transmit(&huart2, firmware_version_response, 36, 0xffff); isConnected = 1; HAL_UART_Transmit(&huart3, dummy, sizeof(dummy), 0xffff); } else { isConnected = 0; } } } }