Hello,
When we set tequlibrium variable on the PalmSens interface, what is the MethodScript codes to implement this settings?
Thank you,
Hello,
When we set tequlibrium variable on the PalmSens interface, what is the MethodScript codes to implement this settings?
Thank you,
The simplest way is to just use "set_e <potential>" to set the required potential, followed by a "wait <time>" command. What PSTrace does is slightly more complicated but it is unlikely to make a difference.
Can I set 500mV as a required potential every time?
If 500 mV is within the range you have provided with the "set_range_minmax da <min> <max>", yes this is fine. If you have no used the "set_range_minmax" it will also be fine in this case, you will be able to apply +/- 1100 mV.