Hello,
I have two problems related of the reading data with chemical sensing. First is that the emstat pico is continuously making measurements. For example, I set 2s interval for total 10s duration measurements for the CA so I expect that I will read six different values, then stop, but the system keeps going on reading so how can I limit number of readings? Second question is that the system does not start reading from 1st index unless I do power off-on the system. For example, in the first run of the reading with sensor, I get results with the index from 1st to 500th, then in the second run of the sensor, I get results with the index from 501st to 1000th, so how can I force the system to start form very beginning in each measurements without power off-on the system?
Thank you,