How to drive MOSFET switches in a cascaded hybrid modular multilevel converter using a half-bridge driver "IR2103S"

Hi guys
I am trying to drive the MOSFET switches in a cascaded hybrid modular multi-level converter as shown in Fig. 1. Fig. 2 is used here to simplify the circuit and to present the problem (let's focus on Fig.2 instead of Fig.1). The type of the MOSFET used is "IRF530N" [https://www.alldatasheet.com/datasheet-pdf/pdf/68169/IRF/IRF530N.html]. Each cell is integrated with half-bridge (called a sub-module) while each pack of sub-modules is integrated with full-bridge (called a module). Each module is connected to the next module (cascaded). The type of the Half-bridge driver used is "IR2103S" [https://www.alldatasheet.com/datasheet-pdf/pdf/84683/IRF/IR2103S.html]. A single IR2103S is used to drive each half-bridge while two of IR2103S are used to drive each full-bridge as shown in Fig. 3 and Fig. 4, respectively. Note that in Proteus software, I have used IR2104S instead of IR2103S (both of them are able to achieve the same function). For each half-bridge (except the last half-bridge used), the wire between the COM pin of "IR2103S" and the source pin of the low-side MOSFET switch is lifted as shown in Fig. 5. Cell voltage=3.4V, Rg=47ohm, a capacitor with 22uf/25V, and DC/DC isolated is used for each half-bridge.

The circuit is operating correctly when I am using only one module (only one full-bridge is used) (i am able to measure the positive and the negative output voltage across the H-bridge).
The problem appears when using two modules in a cascade way (see Fig.5). Connecting the load is necessary in this case to complete the circuit. I noted that I can measure the positive output voltage across the two H-bridges correctly (9.7 to 10.1V) while I can't measure the correct negative output voltage (I got -8.42 V).

I have tested the circuit in the lab and by Proteus software and I got the same results. The Proteus file is attached.

I have two questions:
1) Am I able to use the half-bridge driver (IR2103S) to drive the MOSFETs or I should use an individual driver (such as TLP351H) for each MOSFET?
2) if I can use IR2103S, is there anybody who can help me to figure out where is my mistake and how to connect the circuit correctly?

Thanks in advance

Fig. 1Fig. 2Fig. 3 Fig. 5