Epiq Solutions’ Matchstiq
S10, S11 & S12 define the state-of-the-art in small form factor software defined radio platforms. Building on the success of the award-winning Matchstiq
S1 and Z1 platforms, Matchstiq
S10 provides increased RF flexibility, RF performance, and signal processing capacity, in a smaller and lighter package. The S11 adds the option to use the RF inputs as 2 phase coherent RX inputs. And the S12 extends the lower frequency range down below 1 MHz. Click at the bottom of this document to download the complete flyer.