I'm interested in just the ADAU1761 SigmaDSP and developing with that because the board's connectors provide the expansion I need. Can it be used that way?
ADAU1761
Production
The ADAU1761 is a low power, stereo audio codec with integrated digital audio processing that supports stereo 48 kHz record and playback at 14 mW from...
Datasheet
ADAU1761 on Analog.com
I'm interested in just the ADAU1761 SigmaDSP and developing with that because the board's connectors provide the expansion I need. Can it be used that way?
Yes, the EVM can be used for general SigmaDSP development with SigmaStudio. A clock must be provided to the ADAU1761 and there are two easy ways to do that. Details are in the board manual and there's a quick summary on the Documents Wiki.
Yes, the EVM can be used for general SigmaDSP development with SigmaStudio. A clock must be provided to the ADAU1761 and there are two easy ways to do that. Details are in the board manual and there's a quick summary on the Documents Wiki.