Locale Icon
English
EngineerZone
EngineerZone
Other Products Library
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
    • LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

Other Products Library
Other Products Library
Documents What are the DTM (Direct Test Mode) BLE commands supported by MAX32666?
  • Documents
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD10200: FAQ
  • +AD8436: FAQ
  • 3B01: the connection between the 26-pin and 16 channel.
  • 442 - I cannot find the datasheet for the 442 (old OPAMP Module)
  • 751: old datasheet
  • Ac coupling Vs Dc coupling
  • AC1307E Power Supply input range
  • AD-MSDPD-EVB: Eval Board Datasheet
  • ADATE304 Force Voltage
  • ADATE318: What supply voltage do I use for VDD_THERM?
  • ADMP401 startup
  • ADMP441 output format
  • +ADN2531: Can output be configured as current source?
  • ADN2685: could you send the final datasheet?
  • +ADN2814: FAQ
  • +ADN2816: FAQ
  • ADN2817 error correction
  • ADN2820: Optical fiber communication
  • +ADN2830: FAQ
  • +ADN2871: Differential drive circuit for driving a VCSEL Laser diode.
  • +ADN2872: Is it possible to use 2 laser drivers in parallel to have the modulation current of 130 mA?   
  • ADN2873: Minimum differential signal between the DATAP and DATAN
  • ADN2880: MAX leakage current specification of ADN2880 input
  • +ADN2882 Evaluation Board
  • +ADN4600: FAQ
  • +ADN469xE: FAQ
  • +ADN8831: FAQ
  • ADN8834: Evaluation board difference
  • AN-695 Q&A
  • Aqueous washing of ADI parts?
  • Baking BGA in Tray or trays
  • Baking of parts in a Reel
  • Can ADN4604 do single ended 75Ohm input and output?
  • Can I connect one input to multiple outputs?
  • datasheet 2B35
  • Digital programmable power with 1.8V logic to Vout = 5V
  • Does changing the crosspoint connectivity affect the state of previously configured connections?
  • doubling ADN8810 Iout configuration query (SR#: 1202803)
  • EVAL-AD8436 evaluation board operation with single supply
  • Failure probability for AD8468
  • How can I order Linear Circuit Design Handbook?
  • Maximum Recommended PMU Load Capacitance
  • MTBF-reliability data
  • Package general: What is the pin pitch of LFCSP package?
  • Package: 10 ld Ceramic Flat Package footprints
  • paste mask recommendation
  • PFC controller + LED driver in one package
  • Replacement for PMI119-883
  • RoHS compliant status E
  • RTI-850 RTI products
  • Shelf life for Analog parts
  • Shelf life of drypack used to ship Moisture/Reflow Sensitive Surface Mount Devices
  • The unit of MTTF data on ADI web site
  • transistor counts for a processor to calculate the MTBF
  • unused inputs or outputs?
  • What data rates or range of data rates are supported?
  • What data rates protocols are supported?
  • Where can I find e-book versions on your seminar books to download?
  • which register we can read to know the status of HD
  • Why the Analog Input Current from ?10mA to 10 mA was limited.
  • +#N/A: FAQ
  • +--: FAQ
  • +1-WIRE + I2C MULTI-DEVICE PROGRAMMER: FAQ
  • +125932-HMC675LP3E: FAQ
  • +125932-HMC675LP3E: FAQ
  • 310: FAQ
  • +310: FAQ
  • +73M1X22: FAQ
  • +73S8010C-ILR/F: FAQ
  • +73S8010C-ILR/F: FAQ
  • +78P2351-IGT: FAQ
  • +78Q2123/F: FAQ
  • 78Q2123/F: FAQ
  • +78Q8392LA03-CHR/F: FAQ
  • 78Q8392LA03: FAQ
  • +78Q8392LA03: FAQ
  • +940: FAQ
  • +AD-CELLPACKBM-SL: FAQ
  • +AD-CELLPACKBM-SL: FAQ
  • +AD-GMSL522-SL: FAQ
  • +AD1835: FAQ
  • +AD1835A: FAQ
  • +AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • AD1862
  • AD1862: FAQ
  • +AD1881A: FAQ
  • +AD1937: FAQ
  • +AD1937: FAQ
  • +AD1938: FAQ
  • +AD1939: FAQ
  • +AD1970: FAQ
  • +AD1970: FAQ
  • +AD1970: FAQ
  • +AD1981: FAQ
  • +AD1981B: FAQ
  • AD1986: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +AD22151: FAQ
  • +AD22151: FAQ
  • +AD22282-A-R2: FAQ
  • +AD22290: FAQ
  • +AD4195-4BCPZ: FAQ
  • +AD506: FAQ
  • AD53500: FAQ
  • AD53500: Thermal questions
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • AD5934 questions - measuring inductive reactance
  • +AD5934: FAQ
  • +AD5941: FAQ
  • +AD598JRZ: FAQ
  • +AD630: FAQ
  • +AD630: FAQ
  • +AD644: FAQ
  • +AD6635: FAQ
  • +AD671: FAQ
  • AD7124: FAQ
  • +AD7280: FAQ
  • +AD73311: FAQ
  • +AD73311L: FAQ
  • +AD73322: FAQ
  • AD73322: FAQ
  • +AD73322L: FAQ
  • AD73322L: FAQ
  • +AD74111: FAQ
  • +AD7503: FAQ
  • +AD7503: FAQ
  • +AD7546: FAQ
  • +AD7725: FAQ
  • +AD7756: FAQ
  • AD7756: FAQ
  • +AD8214: FAQ
  • AD8214: FAQ
  • +AD8321: FAQ
  • +AD8324: FAQ
  • +AD8328: FAQ
  • +AD8338: FAQ
  • AD8380: FAQ
  • AD8380: General conditions for various PINS
  • +AD8381: FAQ
  • AD8436 FAQ:
  • AD846 - open loop transimpedance can be reduced?
  • +AD8460: FAQ
  • AD846: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9246S: FAQ
  • +AD9776: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • AD9833: Disconnecting the MCLK
  • +AD9833: FAQ
  • +AD9835: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9838: FAQ
  • +AD9850: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9854ASQ: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9882: FAQ
  • +AD9910: FAQ
  • +AD9910: FAQ
  • +AD9911: FAQ
  • +AD9912: FAQ
  • AD9913: FAQ
  • +AD9914: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9958: FAQ
  • AD9958: FAQ
  • +AD9959: FAQ
  • +ADA4355: FAQ
  • +ADA4355: FAQ
  • ADA4411: FAQ
  • +ADA4411: FAQ
  • +ADAU1381: FAQ
  • +ADAU1461: FAQ
  • +ADAU1701: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • ADE5569: FAQ
  • +ADE5569: FAQ
  • +ADE7752: FAQ
  • +ADE7753: FAQ
  • +ADE7754: FAQ
  • +ADE7756: FAQ
  • ADE7756: FAQ
  • +ADE7757: FAQ
  • +ADE7758: FAQ
  • +ADE7761: FAQ
  • +ADE7763: FAQ
  • +ADE7816: FAQ
  • ADE7854 Apparent Power calculation (AVA)
  • ADE7854: FAQ
  • +ADE7858: FAQ
  • +ADE7868: FAQ
  • +ADE7878: FAQ
  • +ADE7878: FAQ
  • +ADE7880: FAQ
  • +ADE7880: FAQ
  • +ADE7953: FAQ
  • +ADE7953: FAQ
  • +ADE7978: FAQ
  • ADE9078: FAQ
  • +ADE9113: FAQ
  • +ADE9430: FAQ
  • +ADF4360: FAQ
  • +ADF4360: FAQ
  • +ADF5584: FAQ
  • +ADF7001: FAQ
  • +ADF7001: FAQ
  • +ADF7012: FAQ
  • +ADF7012: FAQ
  • +ADF7020: FAQ
  • +ADF7021-N: FAQ
  • +ADF7021-V: FAQ
  • ADF7021-V: FAQ
  • +ADF7021: FAQ
  • +ADF7023: FAQ
  • +ADF7242: FAQ
  • ADF7902: FAQ
  • ADF7902_ EVB doc and software code
  • +ADG201: FAQ
  • ADG324x Level Translation: high to low
  • +ADIN1100CCPZ: FAQ
  • +ADIN6310: FAQ
  • +ADIS16204: FAQ
  • +ADIS16204: FAQ
  • ADIS16300: FAQ
  • +ADIS16355: FAQ
  • +ADIS16400: FAQ
  • +ADIS16400: FAQ
  • +ADISIMPLL: FAQ
  • +ADISUSB: FAQ
  • ADISUSBZ-based software bug Impacts ADIS16300 ADIS1636x ADIS1640x evaluation
  • +ADL5317: FAQ
  • +ADM1030: FAQ
  • ADM1030: FAQ
  • +ADM1031: FAQ
  • ADM3307: FAQ
  • +ADM3307: FAQ
  • +ADM869L: FAQ
  • ADMC300: FAQ
  • +ADMTV315: FAQ
  • ADMV4420 gain reduction
  • ADMV4420: FAQ
  • ADN2890/1/2 at 100Mbps?
  • ADN2892: FAQ
  • +ADP3040: FAQ
  • +ADP3302: FAQ
  • +ADP5046: FAQ
  • +ADPA1112: FAQ
  • ADPA9007: FAQ
  • ADR125: FAQ
  • ADR125: Output Capacitance
  • +ADRF5162: FAQ
  • ADRF5700 lower power supply
  • ADRF5700: FAQ
  • +ADRF6515: FAQ
  • ADRV9361-Z7035 clock input Vih Max, discrepancy
  • +ADRV9361-Z7035: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • ADSP-21363: FAQ
  • +ADSP-21365: FAQ
  • ADSP-21368 - WS Value
  • ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +ADSP-BF533: FAQ
  • ADSP-BF533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF701: FAQ
  • +ADSP-CM408F: FAQ
  • ADSP-TS001: FAQ
  • ADT70: FAQ
  • +ADT70: FAQ
  • +ADT7460: FAQ
  • ADT7460: FAQ
  • +ADT7461: FAQ
  • +ADT7461: FAQ
  • +ADUC7020: FAQ
  • +ADUC7021: FAQ
  • +ADUC7023: FAQ
  • +ADUC7024: FAQ
  • +ADUC7024: FAQ
  • +ADUC7026: FAQ
  • +ADUC7033: FAQ
  • +ADUC7033: FAQ
  • +ADUC7060: FAQ
  • +ADUC7061: FAQ
  • +ADUC7120: FAQ
  • +ADUC7122: FAQ
  • +ADUC7126: FAQ
  • ADUC7128: FAQ
  • ADuC7xxx: Can I read flash/eeprom and reprogram specific addresses via UART?
  • +ADUC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADUC831: FAQ
  • +ADUC832: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADUC836: FAQ
  • +ADUC841: FAQ
  • ADUC841: FAQ
  • +ADUC842: FAQ
  • +ADUC842: FAQ
  • +ADUC843: FAQ
  • +ADUC843: FAQ
  • +ADUC845: FAQ
  • +ADUC847: FAQ
  • +ADUC848: FAQ
  • +ADUCM360: FAQ
  • +ADUCM360: FAQ
  • +ADUCM361: FAQ
  • +ADUCM362: FAQ
  • ADUCM362: FAQ
  • +ADUCM4050: FAQ
  • +ADUCM410: FAQ
  • ADUCM410: FAQ
  • +ADUCRF101: FAQ
  • +ADUM1400: FAQ
  • +ADUM2400: FAQ
  • +ADUM2400: FAQ
  • +ADUM4160: FAQ
  • +ADV7202: FAQ
  • ADV7202: FAQ
  • +ADXL358: FAQ
  • +ADXL365: FAQ
  • +ADXL365: FAQ
  • +ADZS-A2B-HARDWARE: FAQ
  • availability of the ADMC300 devices
  • AWR/ADS Simulation Model for HMC1087F10
  • +CABLE-PH04: FAQ
  • Can a Model Already Pre-Trained in TensorFlow be Converted for Use in the MAX78000?
  • Can ADE7816 be used as Bidirectional Energy Meter and accumulate import and export energy values separately?
  • Can DS21554 support any optical interface?
  • Can I use LTP8802A-1B / DC3190B-F without any air flow moving across it?
  • Can the DS9092 device be used with the DS9490R adapter?
  • Can the PP pin of the TMC5041 be grounded?
  • Can TMC6140 work in closed loop?
  • Can two channel operation with two different references using the AD7124-8?
  • Can we share information on the DSQ2FL1-J00+T?
  • Can we use an external excitation current with the LTC2984?
  • Can we use the TMC6140 Eval-kit with TMC4671?
  • Can we use TMCL firmware with TMCM-1633.
  • Can you replace the crystal with an external clock source on the MAX1472?
  • +CN0196: FAQ
  • CN0287 limitations due to common SPI lines (AD5201 & AD7193)
  • CN0287: FAQ
  • +CN0303: FAQ
  • Could OFFSET pin of the MAX40213 be used for cancelling the DC part of the input current?
  • +DC1075B-B: FAQ
  • +DC1075B-B: FAQ
  • DC1854A: FAQ
  • +DC2039A: FAQ
  • +DC2046A-B: FAQ
  • +DC2393A: FAQ
  • DC2465A: FAQ
  • DC2617A: FAQ
  • +DC9000A: FAQ
  • +DC9018A-C: FAQ
  • +DC9021B: FAQ
  • DC9021B: FAQ
  • +DC9022B: FAQ
  • Definition of 'Reverse isolation' for HMC590LP5
  • Difference in DS2155 and DS26504 recover clock performance?
  • Do we need additional drivers for for TMC USB-2-485 Windows 10 support?
  • Do you have EVAL-HCRWATCH4Z Firmware Source Code available?
  • Do you still have the ZLP32300?
  • Does MAX32660 support boundary scan?
  • Does MAX32668 support LE software profiles like HFP V1.5, A2DP V1.2, AVRCP V1.4, GAVDP V1.2, AVDTP V1.2, SPP V1.2, AVCTP V1.2?
  • Does the MAX32655 support BLE4.2?
  • Does Trinamic have any parts to operate a sensorless BLDC?
  • +DS1010B UNTESTED RAW DIE: FAQ
  • +DS1181LE+: FAQ
  • DS1225AB-150: FAQ
  • +DS1225AB-150IND+: FAQ
  • +DS1225AD-200IND: FAQ
  • DS1230Y-70IND+: FAQ
  • +DS1230Y: FAQ
  • +DS1235A: FAQ
  • +DS1236 UNTESTED UNLASERED DIE: FAQ
  • +DS1267-010: FAQ
  • +DS1267-10 UNTESTED RAW DIE: FAQ
  • DS1267-10 UNTESTED RAW DIE: FAQ
  • +DS1270Y-70#: FAQ
  • +DS1270Y-70IND#: FAQ
  • +DS1312+: FAQ
  • +DS1402 BUTTON TO RJ11 PLUG CABLE: FAQ
  • +DS1402-RP8+: FAQ
  • +DS1402D-DR8+: FAQ
  • +DS1410E: FAQ
  • +DS1644-120: FAQ
  • +DS1669N-010: FAQ
  • +DS1669N-010: FAQ
  • +DS1821C+: FAQ
  • +DS1821C+: FAQ
  • +DS1856B-020+: FAQ
  • DS1856B-020+: FAQ
  • +DS1856M: FAQ
  • +DS1859: FAQ
  • +DS1875K#: FAQ
  • +DS1904L-F5#: FAQ
  • +DS1920-F5+: FAQ
  • +DS1921: FAQ
  • +DS1922: FAQ
  • +DS1954: FAQ
  • +DS1954: FAQ
  • +DS1961S: FAQ
  • DS1961S: FAQ
  • DS1963S: FAQ
  • +DS1971-F5+: FAQ
  • +DS1971-F5+: FAQ
  • +DS1973-F3+: FAQ
  • +DS1977-F5#: FAQ
  • +DS1990A-019-F5A#CB: FAQ
  • +DS1990A-F3+: FAQ
  • +DS1990A-F3+: FAQ
  • +DS1990A-F5+: FAQ
  • +DS1991: FAQ
  • +DS1993: FAQ
  • DS21554: FAQ
  • +DS2155DK: FAQ
  • +DS2155LNC2+: FAQ
  • +DS2482S-100+: FAQ
  • +DS2482S-800+T&R: FAQ
  • +DS2482S-800+T&R: FAQ
  • +DS2483: FAQ
  • +DS2490: FAQ
  • +DS2490S+: FAQ
  • +DS2506: FAQ
  • +DS26502DK: FAQ
  • +DS26502L+: FAQ
  • DS26502L+: FAQ
  • +DS26504: FAQ
  • DS26504L+: FAQ
  • +DS26514GN+: FAQ
  • DS26518DK: FAQ
  • +DS26518DK: FAQ
  • +DS26518G+: FAQ
  • +DS26518GN+: FAQ
  • +DS26521: FAQ
  • DS26521: FAQ
  • +DS26521L+: FAQ
  • +DS28CN01: FAQ
  • +DS28CN01: FAQ
  • +DS28E01: FAQ
  • DS28E04S-100+: FAQ
  • +DS28E11P+: FAQ
  • +DS3150TN+: FAQ
  • +DS3177+: FAQ
  • +DS34S132: FAQ
  • DS34S132: FAQ
  • +DS34T101: FAQ
  • +DS34T101GN+: FAQ
  • DS34T104: FAQ
  • +DS34T108GN+: FAQ
  • +DS3911: FAQ
  • +DS3935VGTL+: FAQ
  • +DS4100H+: FAQ
  • +DS4100H+: FAQ
  • +DS4125: FAQ
  • +DS4125: FAQ
  • +DS4830A: FAQ
  • DS4830A: FAQ
  • +DS4830AEVKIT: FAQ
  • +DS4830AT+: FAQ
  • +DS75S-C1+T&R: FAQ
  • DS80C320: FAQ
  • +DS80C320: FAQ
  • +DS80C323-ECD+: FAQ
  • +DS80C400-KIT: FAQ
  • +DS89C430-ENL+: FAQ
  • +DS89C430: FAQ
  • +DS89C450-ENG+: FAQ
  • +DS89C450-QNG+: FAQ
  • +DS9034PC+: FAQ
  • DS9034PC+: FAQ
  • +DS9034PCX+: FAQ
  • +DS9072: FAQ
  • +DS9090EVKIT#: FAQ
  • DS9092+: FAQ
  • +DS9092L+: FAQ
  • +DS9093S+: FAQ
  • +DS9097U-009#: FAQ
  • +DS9097U-E25: FAQ
  • +DS9097U-S09#: FAQ
  • +DS9107+: FAQ
  • +DS9120P+: FAQ
  • DS91230: FAQ
  • +DS91230: FAQ
  • +DS9481P-300#: FAQ
  • DS9481P-300#: FAQ
  • +DS9490B#: FAQ
  • +DS9490R#: FAQ
  • +DS9503P+: FAQ
  • DSQ2FL1-J00+T: FAQ
  • dynamically turn off and on the instruction and/or data
  • +EV-ADAQ7769-1FMC1Z: FAQ
  • +EV1HMC994APM5: FAQ
  • EVAL-CN0566-RPIZ: FAQ
  • EVAL-HCRWATCH4Z: FAQ
  • +EVAL-PRAOPAMP: FAQ
  • Execution error 13  Type incompatible
  • HMC1087: FAQ
  • +HMC1114: FAQ
  • HMC342G: FAQ
  • HMC518: FAQ
  • +HMC518: FAQ
  • HMC590: FAQ
  • +HMC6000: FAQ
  • +HMC605LP3E: FAQ
  • +HMC624: FAQ
  • +HMC6300G: FAQ
  • HMC757: FAQ
  • +HMC852: FAQ
  • +HMC930A: FAQ
  • +HMC994A: FAQ
  • +HMC994A: FAQ
  • How can I measure an unmodulated signal from MAX41463?
  • How can we read the encoder scale index in TMC457?
  • How should the AD8460 evaluation board be set up and troubleshot if the AWG mode output fails to refresh?
  • How to obtain 2nd harmonic data for the ADPA9007 part outside of the Pout range specified in the datasheet?
  • How to open .PCB files of some of the Demoboards using Linear Technology parts (e.g. DC2465A-2.PCB file)?
  • How to use SAToP to provide channelized T1 services. If framer is set as SF/ESF mode, and the bundle is configued as unstructure type(SATOP), will DS34T104 chip work correctly? How does the chip locate the f bit and timeslot into frame?
  • How-to connect a Raspberry Pi Camera Module 2 to the AD-GMSL522-SL
  • +HSC-ADC-EVALB-DC: FAQ
  • +HSC-ADC-EVALC: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • HSC-ADC-EVALCZ: FAQ
  • HSC_ADC_EVALCZ_J9 setup-1
  • +HSC_EVALBOARD: FAQ
  • +HSC_EVALBOARD: FAQ
  • I am using a Whaleteq PPG simulator with the MAXREFDES105, and have noticed that it has poor results in the range 30 - 60BPM. Whereas for inputs over 60BPM, it shows good accuracy. Why is this?
  • I2S interface configuration
  • IA188EBPLC84IR2: FAQ
  • +IC0400C778BF+LTB: FAQ
  • Is is possible to use the ADE9078 3ph meter in a 1ph metering application?
  • Is it possible to create Standalone TMCM Module using CANopen ?
  • Is it possible to get your EVAL-CN0566-RPIZ (Phaser) software to work with Kuiper Linux 2023\_r2?
  • Is It Possible to Implement Intermittent Computing with MAX78000FTHR?
  • Is it possible to program the LTP5902-WHM WirelessHART module via UART?
  • Is it possible to update the firmware of PD42-1-1243-IOLINK stepper motor, which has old hardware version 1.0?
  • Is it possible to use ISM band transceivers like the MAX1479/MAX1470 for musical instruments?
  • Is there a battery internal to the DS1963S device?
  • Is there a specific part of MAX32651 RAM that is known to be untouched by the secure bootloader?
  • Is there a TMCL command to return the TMC module number? e.g. TMCM-3110 vs TMCM-6214?
  • Is there an EMC Report available for the DS1230Y-70IND?
  • +LM75BIMM-3+: FAQ
  • LT4256-2: FAQ
  • LT8471 Demo Board DC1854A Input Voltage Range
  • LTC2984: FAQ
  • +LTC2991: FAQ
  • +LTC3310: FAQ
  • LTC3310: FAQ
  • +LTC4162: FAQ
  • +LTC4162: FAQ
  • +LTC7000: FAQ
  • +LTM4654: FAQ
  • +LTM4739: FAQ
  • LTP5900-WHM: FAQ
  • +LTP5900-WHM: FAQ
  • LTP5902-WHM: FAQ
  • LTP8802: FAQ
  • +LTpowerCAD: FAQ
  • +LTSPICE: FAQ
  • +MAX-ECG-MONITOR: FAQ
  • +MAX-HEALTH-BAND: FAQ
  • +MAX-HEALTHBAND: FAQ
  • MAX038CWP+_T1: FAQ
  • +MAX038CWP+_T1: FAQ
  • +MAX104CHC: FAQ
  • MAX1377: FAQ
  • +MAX14648: FAQ
  • +MAX1464EVKIT: FAQ
  • +MAX1472: FAQ
  • MAX1472AKA+T: FAQ
  • MAX1479ATE+: FAQ
  • +MAX15500: FAQ
  • MAX15500: FAQ
  • +MAX21000+TWCHS: FAQ
  • +MAX21001/V+: FAQ
  • +MAX2150ETI+: FAQ
  • +MAX2242: FAQ
  • +MAX2242: FAQ
  • +MAX235CPG+G36: FAQ
  • +MAX235MDG/HR: FAQ
  • +MAX2654EXT+: FAQ
  • MAX2654EXT+: FAQ
  • +MAX274A: FAQ
  • +MAX274EVKIT-DIP+: FAQ
  • +MAX28200EWC+T: FAQ
  • +MAX28200EWC+TC02: FAQ
  • +MAX2828ETN+T: FAQ
  • +MAX2829ETN+: FAQ
  • +MAX2830: FAQ
  • +MAX2830ETM+T: FAQ
  • +MAX2831: FAQ
  • +MAX2831EVKIT: FAQ
  • +MAX2837ETM+: FAQ
  • +MAX2837ETM+: FAQ
  • +MAX2837EVKIT+: FAQ
  • +MAX2850: FAQ
  • +MAX2851ITK+: FAQ
  • +MAX2900ETI+: FAQ
  • +MAX291: FAQ
  • +MAX291: FAQ
  • +MAX2990ECB+: FAQ
  • +MAX2992: FAQ
  • +MAX30034CTA+: FAQ
  • +MAX30034CUA+: FAQ
  • +MAX31856MUD+: FAQ
  • MAX31856MUD+: FAQ
  • +MAX32510: FAQ
  • +MAX32520/W+JU: FAQ
  • MAX32520/W+JU: FAQ
  • +MAX32520ATJJ/V+: FAQ
  • +MAX32550: FAQ
  • +MAX32550: FAQ
  • +MAX32552-LCJ+: FAQ
  • MAX32552-LCJ+: FAQ
  • +MAX32555/B+: FAQ
  • +MAX32555: FAQ
  • MAX32555: FAQ
  • +MAX32558: FAQ
  • +MAX32560: FAQ
  • +MAX32590-LNS+: FAQ
  • +MAX32620-EVKIT#: FAQ
  • +MAX32620FTHR#: FAQ
  • +MAX32620ICQ+: FAQ
  • +MAX32620ICQ+: FAQ
  • +MAX32620IWG+: FAQ
  • +MAX32620IWG+T: FAQ
  • +MAX32621-EVKIT#: FAQ
  • +MAX32621IWG+T: FAQ
  • +MAX32625-EVKIT#: FAQ
  • +MAX32625ITK+: FAQ
  • +MAX32625MBED#: FAQ
  • MAX32625MBED#: FAQ
  • +MAX32625NEXPAQ: FAQ
  • +MAX32625NEXPAQ: FAQ
  • +MAX32625PICO#: FAQ
  • +MAX32626-EVKIT#: FAQ
  • +MAX32626-EVKIT: FAQ
  • +MAX32626-EVKIT: FAQ
  • +MAX32630-EVKIT#: FAQ
  • +MAX32630FTHR#: FAQ
  • +MAX32630ICQ+: FAQ
  • +MAX32630IWG+: FAQ
  • +MAX32630IWG+T: FAQ
  • +MAX32631-EVKIT#: FAQ
  • +MAX32631ICQ+: FAQ
  • MAX32631ICQ+: FAQ
  • +MAX32632: FAQ
  • +MAX32650-EVKIT#: FAQ
  • +MAX32650EVKIT: FAQ
  • +MAX32650GCE+: FAQ
  • +MAX32650GWQ+T: FAQ
  • +MAX32651GCE+: FAQ
  • +MAX32652: FAQ
  • MAX32652: FAQ
  • MAX32655GWY+: FAQ
  • +MAX32660-EVKIT#: FAQ
  • +MAX32660-EVKIT: FAQ
  • +MAX32660-EVSYS#: FAQ
  • +MAX32660EVKIT: FAQ
  • +MAX32660GTG+T: FAQ
  • +MAX32660GTGBL+: FAQ
  • +MAX32660GTGLA+T: FAQ
  • +MAX32660GWE+: FAQ
  • +MAX32665EVKIT#: FAQ
  • +MAX32665EVKIT#: FAQ
  • +MAX32665GXMBT+T: FAQ
  • MAX32665GXMBT+T: FAQ
  • +MAX32666FTHR#: FAQ
  • +MAX32666GWP+: FAQ
  • +MAX32666GWPBT+: FAQ
  • MAX32666GWPBT+: FAQ
  • +MAX32666GWPBT+T: FAQ
  • MAX32668GWPBL+: FAQ
  • +MAX32670GTL+: FAQ
  • +MAX3421: FAQ
  • +MAX34461AA00+: FAQ
  • +MAX34461AA00+: FAQ
  • +MAX34463EXQA3+: FAQ
  • +MAX3600: FAQ
  • MAX3600: FAQ
  • +MAX3601GTL+: FAQ
  • +MAX3634: FAQ
  • +MAX3634: FAQ
  • +MAX3668: FAQ
  • +MAX3711: FAQ
  • MAX3711: FAQ
  • MAX3735AE/D: FAQ
  • +MAX3735AE/D: FAQ
  • +MAX3735AETG+: FAQ
  • +MAX3736ETE+: FAQ
  • +MAX3738: FAQ
  • +MAX3740AETG+: FAQ
  • +MAX3740AETG+: FAQ
  • +MAX3747AEUB+: FAQ
  • +MAX3747AEUB+: FAQ
  • +MAX3748HETE+: FAQ
  • +MAX3748HETE+: FAQ
  • +MAX3761: FAQ
  • +MAX3869EHJ+: FAQ
  • +MAX3869EHJ+T: FAQ
  • +MAX40056EVKIT#: FAQ
  • MAX40213: FAQ
  • +MAX4137: FAQ
  • +MAX41460EVKIT: FAQ
  • +MAX41460GUB+: FAQ
  • +MAX41461GUB+T: FAQ
  • MAX41463GUB+: FAQ
  • +MAX4207: FAQ
  • +MAX4207: FAQ
  • +MAX5859EXW-D: FAQ
  • +MAX5859EXW-D: FAQ
  • +MAX5933AESA+: FAQ
  • +MAX5965: FAQ
  • +MAX5974: FAQ
  • +MAX5988A: FAQ
  • MAX6682MUA+T: FAQ
  • MAX6839XSD2+: FAQ
  • +MAX7030HATJ+: FAQ
  • +MAX7032: FAQ
  • +MAX7037EGL+T: FAQ
  • MAX7037EGL+T: FAQ
  • +MAX7037EVKIT#: FAQ
  • +MAX7474EAE+_T1: FAQ
  • +MAX77729XEWN+: FAQ
  • +MAX77729XEWN+: FAQ
  • +MAX77823EWZ+: FAQ
  • +MAX77859AEWO+: FAQ
  • MAX77932 cannot power up successfully when Vin ramp up slowly, how to solve the problem?
  • MAX77932BEWO+: FAQ
  • +MAX77932EWO+T: FAQ
  • +MAX77932EWO+T: FAQ
  • +MAX77972: FAQ
  • +MAX78000EXG+: FAQ
  • +MAX78000FTHR: FAQ
  • +MAX78700: FAQ
  • +MAX8790AETP+: FAQ
  • MAX8804: FAQ
  • +MAX881: FAQ
  • +MAX8902: FAQ
  • +MAX8903: FAQ
  • +MAX9272: FAQ
  • +MAX9295AGTJ/V+: FAQ
  • +MAX9295EGTN/V+T: FAQ
  • +MAX9296AGTM/V+: FAQ
  • +MAX98089ETN+: FAQ
  • MAX98089ETN+: FAQ
  • +MAX98089EVKIT#WLP: FAQ
  • +MAX98090AETL+: FAQ
  • +MAX98090AETL+T: FAQ
  • +MAX98090AETL+T: FAQ
  • +MAX98090AEWJ+: FAQ
  • +MAX98090EVKIT#WLP: FAQ
  • +MAX98090EVKIT#WLP: FAQ
  • +MAX98091: FAQ
  • +MAX9860ETG+: FAQ
  • +MAX9867: FAQ
  • +MAX9867ETJ+: FAQ
  • MAX9867ETJ+: FAQ
  • +MAX9867EVKIT+: FAQ
  • MAX9880A: FAQ
  • +MAX9880A: FAQ
  • +MAX9880AETM+: FAQ
  • +MAX9880AEVKIT#: FAQ
  • +MAX9947ETE+: FAQ
  • +MAXADCLITE+: FAQ
  • +MAXCOAX2STP-HSD#: FAQ
  • +MAXPOWERTOOL002#: FAQ
  • +MAXQ1741: FAQ
  • +MAXQ1743: FAQ
  • +MAXQ1744-DNS+: FAQ
  • +MAXQ1744-DNS+: FAQ
  • +MAXQ617: FAQ
  • +MAXQ7667AACM/V+: FAQ
  • +MAXQUSBJTAGOW-KIT#: FAQ
  • +MAXREFDES100#: FAQ
  • +MAXREFDES101 SOFTWARE FOR WINDOWS 10: FAQ
  • +MAXREFDES101#: FAQ
  • +MAXREFDES103#: FAQ
  • +MAXREFDES104#: FAQ
  • +MAXREFDES104: FAQ
  • +MAXREFDES104: FAQ
  • +MAXREFDES105#: FAQ
  • +MAXREFDES106: FAQ
  • +MAXREFDES117#: FAQ
  • +MAXREFDES132#: FAQ
  • +MAXREFDES145#: FAQ
  • +MAXREFDES150#: FAQ
  • +MAXREFDES16#: FAQ
  • +MAXREFDES165#: FAQ
  • +MAXREFDES212#: FAQ
  • +MAXREFDES220#: FAQ
  • +MAXREFDES280: FAQ
  • +MAXREFDES31#: FAQ
  • MAXREFDES31#: FAQ
  • +MAXREFDES37#: FAQ
  • +MAXREFDES4#: FAQ
  • +MAXREFDES42#: FAQ
  • +MAXREFDES70#: FAQ
  • +MAXREFDES73#: FAQ
  • +MAXREFDES74#: FAQ
  • +MAXREFDES74: FAQ
  • +MAXREFDES77#: FAQ
  • +MAXREFDES79#: FAQ
  • MAXREFDES79#: FAQ
  • +MINIQUSB: FAQ
  • +NO PART NUMBER: FAQ
  • NO PART NUMBER: FAQ
  • +NONE: FAQ
  • +OP07: FAQ
  • +OP90: FAQ
  • OP90: FAQ
  • +PCB, MAX2850EVKIT+: FAQ
  • +PD20-1-1210: FAQ
  • +PD20-1-1210: FAQ
  • +PD28-3-1021-TMCL: FAQ
  • +PD42-1-1140-TMCL: FAQ
  • PD42-1-1243-IOLINK: FAQ
  • +PD42-1-1370-TMCL: FAQ
  • +PD42-1-1370-TMCL: FAQ
  • +PD42-4-1370-TMCL: FAQ
  • PD42-4-1370-TMCL: FAQ
  • +PD57-1-1076: FAQ
  • +PD57-1-1160-TMCL: FAQ
  • +PD57-1-1160-TMCL: FAQ
  • +PD57-1-1260-TMCL: FAQ
  • +PD57-1-1378-CANOPEN: FAQ
  • PD57-2-1160-TMCL: FAQ
  • +PD60-3-1260-TMCL: FAQ
  • +PH-MODULES-TRINAMIC: FAQ
  • +PH-MODULES-TRINAMIC: FAQ
  • Porting a VDK-project from Visual DSP++ 3.5 to 4.0
  • Problems with emulator session using floating license for VisualDSP++ 4.0?
  • +QBL4208-100-04-025: FAQ
  • +QBL4208-41-04-006: FAQ
  • QBL4208-61-04-013: FAQ
  • +QBL5704-116-04-042: FAQ
  • +QSH2818-32-07-006: FAQ
  • +QSH4218-41-10-035: FAQ
  • +Questions
  • +REF02A: FAQ
  • RF performance of HMC757LP4E beyond recomended Freq range of operation
  • +RS485: FAQ
  • S Parameters for HMC342LC4 at bias condition 3.3V
  • +SC-USB-SPI: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2602: FAQ
  • SSM2603 audio codec power supply questions
  • SSM2603: FAQ
  • +STM1E-SFP02: FAQ
  • +STM1E-SFP22: FAQ
  • +STM1E-SFP22: FAQ
  • +SW02: FAQ
  • +TEST: FAQ
  • TMC USB-2-485: FAQ
  • TMC2041-EVAL: FAQ
  • +TMC2041-EVAL: FAQ
  • +TMC2041-LA: FAQ
  • +TMC2130-LA: FAQ
  • +TMC2208SILENTSTEPSTICK: FAQ
  • +TMC2209 SILENTSTEPSTICK: FAQ
  • +TMC2209-LA-T: FAQ
  • +TMC2209-LA: FAQ
  • +TMC2209-LA: FAQ
  • +TMC2226-BOB: FAQ
  • TMC2226-BOB: FAQ
  • +TMC2240: FAQ
  • +TMC2240: FAQ
  • +TMC2590: FAQ
  • TMC2590: FAQ
  • +TMC262: FAQ
  • +TMC262C-LA: FAQ
  • TMC2660C-PA-T: FAQ
  • +TMC2660C-PA: FAQ
  • +TMC429-I: FAQ
  • +TMC4361A-LA: FAQ
  • TMC4361A-LA: FAQ
  • TMC457: FAQ
  • +TMC4671: FAQ
  • +TMC5031: FAQ
  • +TMC5041-LA: FAQ
  • +TMC5062-LA: FAQ
  • +TMC5072-LA: FAQ
  • +TMC5130-EVAL-KIT: FAQ
  • +TMC5130A-TA: FAQ
  • TMC5130A-TA: FAQ
  • TMC5160 SILENTSTEPSTICK: FAQ
  • +TMC5160 SILENTSTEPSTICK: FAQ
  • +TMC5160-BOB: FAQ
  • +TMC5160-BOB: FAQ
  • TMC5160-EVAL: FAQ
  • +TMC5160A-TA: FAQ
  • +TMC5240: FAQ
  • TMC5272-EVAL-KIT: FAQ
  • TMC6140-EVAL: FAQ
  • TMC6140: FAQ
  • +TMC8462: FAQ
  • +TMCM-1043: FAQ
  • +TMCM-1043: FAQ
  • +TMCM-1070: FAQ
  • +TMCM-1070: FAQ
  • +TMCM-110-42-485: FAQ
  • TMCM-110-42-485: FAQ
  • +TMCM-1110 STEPROCKER: FAQ
  • +TMCM-1140-TMCL: FAQ
  • +TMCM-1140-TMCL: FAQ
  • +TMCM-1160-TMCL: FAQ
  • +TMCM-1180-TMCL: FAQ
  • +TMCM-1240: FAQ
  • +TMCM-1260-CANOPEN: FAQ
  • +TMCM-1260-TMCL: FAQ
  • +TMCM-1270-CANOPEN: FAQ
  • TMCM-1270-CANOPEN: FAQ
  • +TMCM-1290: FAQ
  • +TMCM-1290: FAQ
  • +TMCM-142-IF-TMCL: FAQ
  • TMCM-142-IF-TMCL: FAQ
  • +TMCM-1630-2C: FAQ
  • +TMCM-1630-2C: FAQ
  • TMCM-1630-4U: FAQ
  • +TMCM-1633-CANOPEN: FAQ
  • TMCM-1633: FAQ
  • +TMCM-1636-24V-CANOPEN: FAQ
  • +TMCM-1640: FAQ
  • +TMCM-1690: FAQ
  • +TMCM-310/SG: FAQ
  • TMCM-310/SG: FAQ
  • +TMCM-3110-TMCL: FAQ
  • +TMCM-3212-TMCL: FAQ
  • +TMCM-3230-TMCL: FAQ
  • +TMCM-3314: FAQ
  • +TMCM-3351-TMCL: FAQ
  • +TMCM-6110: FAQ
  • +TMCM-6212-TMCL: FAQ
  • +TMCM-6212: FAQ
  • +TMCM-6214-CANOPEN: FAQ
  • +TMCM-6214-CANOPEN: FAQ
  • +TMCM-6214-TMCL: FAQ
  • +TMCS: FAQ
  • +TRINAMIC MISC SERVICE: FAQ
  • +TRINAMIC MISC SERVICE: FAQ
  • +TRINAMIC PACKAGING SURCHARGE: FAQ
  • +USB-2-RTMI: FAQ
  • USB2GPIO#: FAQ
  • +USB2GPIO#: FAQ
  • +USB2PMB2#: FAQ
  • +VDSP-BLKFN-PC-FULL: FAQ
  • VDSP-TS-PC-FULL: FAQ
  • +VISUALAUDIO: FAQ
  • +VT202: FAQ
  • +VT273SAFQ: FAQ
  • VT273SAFQ: FAQ
  • What accelerometers are supported by the MAX32664C firmware?
  • What are potential causes for a damaged Trinamic motor driver IC (burnt near pins)? TMC2660C, TMC260C, TMC261C, TMC246, TMC236
  • What are the DTM (Direct Test Mode) BLE commands supported by MAX32666?
  • What does the "S" denote in DS28E04S?
  • What examples are included in the MAX32630/31/32 SDK?
  • What is the default value of one revolution in TMC4671 ?
  • What is the difference between a Thermistor and an RTD?
  • What is the recommended socket base for DS1225AB ?
  • What is the tolerance on the 5mm shaft of the QBL4208-61-04-013 motor?
  • What is the unit for Telegram Pause Time (Global Parameter 75)?
  • When attempting to update the PD57-2-1160 it loses connection and fails, is there a fix for this?
  • Where can I download the technical documents (such as the datasheet) for the IA188EBPLC84IR2?
  • Where Can I Find Design Files for Trinamic's SilentStepSticks?
  • Where can I find the CAN address table for the DC2617A?
  • Where can I find the user manual for TMC5160-eval?
  • Which communication protocol, SPI or UART, is best suited with Direct_mode?
  • Why does the LT4256-2 turn OFF the GATE during dynamic load testing with fast current spikes, without triggering the TIMER?
  • Why does the MAX8804 chip turn off the output when input voltage is above 7.5V?
  • Why is MAX6389LT28D2+ bench measured reset timeout inconsistent with specification?
  • Why is the Encoder Deviation feature of the PD60-3-1260 not working for any value under 40 steps (using 256 microstepping)?
  • Why is the TMC5272-Eval not running even if the set up is correct?
  • With two TMCM-6214 modules on the same RS485 bus I can only see one in the TMCL-IDE, why the second one does not show up?
  • ZLP32300: FAQ
  • +_DS9093A: FAQ
  • +_DS9093A: FAQ

What are the DTM (Direct Test Mode) BLE commands supported by MAX32666?

The DTM mode will accept the commands outlined in the Bluetooth Core Specification 5.0, Vol 2, Part E, Section 7.

The direct test mode commands, outlined in Vol 6, Part F, are also accepted.

There are Maxim-implemented Vendor Specific commands that would also be useful in this context:

#define HCI_OPCODE_VS_SET_BD_ADDR HCI_OPCODE(HCI_OGF_VENDOR_SPEC, 0x3F0)

#define HCI_OPCODE_VS_SET_TX_POWER HCI_OPCODE(HCI_OGF_VENDOR_SPEC, 0x3D4)

The VS_SET_BD_ADDR command accepts an 8-byte address for the new address of the device.

The VS_SET_TX_POWER command accepts a single byte.