Question:
Answer:
- Can the ADRF5700 be capable of operating with a single power supply, exhibiting only a minor degradation of approximately 0.1 dB and third-order intercept—both of which are not critical for the intended application.
- what potential performance loss may occur if the device is supplied with 3.0 V instead of the recommended minimum of 3.15 V?
Answer:
- Typically, there will be around +/-5% variation for the bias supply, which is +3.15V to +3.45V for Vdd.
- If operate with +3V instead of +3.15V, there will be extra insertion loss compared to the +3.15V case. Moreover, the IP3 will degrade but it is not critical for their application.