All of our dedicated stepper motor drivers are designed for use with bipolar stepper motors. There is a small chance that the unipolar motor can be operated like a bipolar motor, depending on the coil terminations. If the middle tap of both motor coils are visible externally, then simply separating this connection will allow the TMCM-1070 driver to be connected to the motor coils in a bipolar fashion.