Yes, an example writting the flash is provided in the SDK in the Applications sub-folder titled, Flash. The SDK/API can be downloaded using the ARMCortexToolchain installer. You can easily choose to download only the product specific resources/firmware. The folder is located in <MYINSTALLDIR>\Firmware\MAX32650\Applications\EvKitExamples\Flash