The only drivers available are for the Linux distribution. Note that this driver has been “upstreamed” to the kernel.org community – so it is part of the Linux kernel as of 2.6.39. Versions of the driver will keep sync with the kernel.
Linux kernel releases are the best place to obtain versions of the driver newer than 2.6.39.