Question:
Unable to establish a connection between ADRV9002 and TES.
Answer:
To establish a proper connection, ensure that the SD card image is not corrupted.
Use PuTTY to initiate a session with the following configuration:
IP Address: 192.168.1.10
Port: 22
Username:
rootPassword:
analog
Verify connectivity by successfully pinging the evaluation board using the Command Prompt (CMD).
For Complete Setup Recommendations:
Please refer to the User Guide available at analog.com/ADRV9002.
Detailed instructions for each component of the platform setup can be found in the "ADRV9001 Evaluation Setup" chapter.