The actual motor position can not be stored in the EEPROM automatically/directly. It can be done via global parameter 2. To achieve this, we recommend to use the AGP command with STGP. After the POR use RSGP and SAP to restore the actual position back.
The same process can be done with other PANdrive modules that share the same parameters and EEPROM functionality.