The MAX5971 determines current limit per the classification. It can be overwritten to a lower classification level (ex. from Class4 to Class3). However, it cannot support further current limit change, for example, from 30W to 18W. The next limit has to be 15.4W.