The body diodes of the internal FETs will clamp positive voltages applied to the M1 and M2 pins when they are above Vdd + 0.3V. If higher voltages are applied to these pins, you must ensure that these voltages do not allow for current greater than 3A to flow into the M1/M2 pins - otherwise damage will occur.