Power Management Fundamentals II Session 6: Key Layout Considerations for Power

    Understand the physics of printed circuit boards to manage large changes in current or voltage. See how layout tweaks can make big improvements for your...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3

    Noise analysis of a circuit requires tracking several things simultaneously: each noise source, how those noise sources are shaped by the circuit, and...

     

    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

    Latest Blogs

    • Achieving Power Over Data with RS-485 Transceivers
    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
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
Other Products (EN)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other Products (EN)
Other Products (EN)
Documents When I measure the Deep Sleep current on the MAX32660, I measure higher than the datasheet value. How can I verify the datasheet value?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD10200: FAQ
  • +AD8436: FAQ
  • 3B01: the connection between the 26-pin and 16 channel.
  • 442 - I cannot find the datasheet for the 442 (old OPAMP Module)
  • 751: old datasheet
  • Ac coupling Vs Dc coupling
  • AC1307E Power Supply input range
  • AD-MSDPD-EVB: Eval Board Datasheet
  • ADATE304 Force Voltage
  • ADATE318: What supply voltage do I use for VDD_THERM?
  • ADMP401 startup
  • ADMP441 output format
  • +ADN2531: Can output be configured as current source?
  • ADN2685: could you send the final datasheet?
  • +ADN2814: FAQ
  • +ADN2816: FAQ
  • ADN2817 error correction
  • ADN2820: Optical fiber communication
  • +ADN2830: FAQ
  • +ADN2871: Differential drive circuit for driving a VCSEL Laser diode.
  • +ADN2872: Is it possible to use 2 laser drivers in parallel to have the modulation current of 130 mA?   
  • ADN2873: Minimum differential signal between the DATAP and DATAN
  • ADN2880: MAX leakage current specification of ADN2880 input
  • +ADN2882 Evaluation Board
  • +ADN4600: FAQ
  • +ADN469xE: FAQ
  • +ADN8831: FAQ
  • ADN8834: Evaluation board difference
  • AN-695 Q&A
  • Aqueous washing of ADI parts?
  • Baking BGA in Tray or trays
  • Baking of parts in a Reel
  • Can ADN4604 do single ended 75Ohm input and output?
  • Can I connect one input to multiple outputs?
  • datasheet 2B35
  • Digital programmable power with 1.8V logic to Vout = 5V
  • Does changing the crosspoint connectivity affect the state of previously configured connections?
  • doubling ADN8810 Iout configuration query (SR#: 1202803)
  • EVAL-AD8436 evaluation board operation with single supply
  • Failure probability for AD8468
  • How can I order Linear Circuit Design Handbook?
  • Maximum Recommended PMU Load Capacitance
  • MTBF-reliability data
  • Package general: What is the pin pitch of LFCSP package?
  • Package: 10 ld Ceramic Flat Package footprints
  • paste mask recommendation
  • PFC controller + LED driver in one package
  • Replacement for PMI119-883
  • RoHS compliant status E
  • RTI-850 RTI products
  • Shelf life for Analog parts
  • Shelf life of drypack used to ship Moisture/Reflow Sensitive Surface Mount Devices
  • The unit of MTTF data on ADI web site
  • transistor counts for a processor to calculate the MTBF
  • unused inputs or outputs?
  • What data rates or range of data rates are supported?
  • What data rates protocols are supported?
  • Where can I find e-book versions on your seminar books to download?
  • which register we can read to know the status of HD
  • Why the Analog Input Current from ?10mA to 10 mA was limited.
  • +#N/A: FAQ
  • +--: FAQ
  • +1-WIRE + I2C MULTI-DEVICE PROGRAMMER: FAQ
  • +125932-HMC675LP3E: FAQ
  • 1s74: FAQ
  • +310: FAQ
  • +73M1X22: FAQ
  • +73S8010C-ILR/F: FAQ
  • +78P2351-IGT: FAQ
  • +78Q2123/F: FAQ
  • +78Q8392LA03-CHR/F: FAQ
  • +940: FAQ
  • +AD-CELLPACKBM-SL: FAQ
  • +AD-GMSL522-SL: FAQ
  • AD1835: FAQ
  • +AD1835A: FAQ
  • AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1862: FAQ
  • +AD1881A: FAQ
  • +AD1937: FAQ
  • +AD1938: FAQ
  • +AD1939: FAQ
  • +AD1970: FAQ
  • AD1981: FAQ
  • +AD1981B: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +AD22151: FAQ
  • +AD22282-A-R2: FAQ
  • +AD22290: FAQ
  • +AD506: FAQ
  • +AD53500: FAQ
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD598JRZ: FAQ
  • +AD630: FAQ
  • +AD644: FAQ
  • +AD6635: FAQ
  • +AD671: FAQ
  • +AD7124: FAQ
  • +AD7280: FAQ
  • +AD73311: FAQ
  • +AD73311L: FAQ
  • AD73322: FAQ
  • +AD73322L: FAQ
  • +AD74111: FAQ
  • +AD7503: FAQ
  • +AD7546: FAQ
  • +AD7725: FAQ
  • +AD7756: FAQ
  • +AD8036: FAQ
  • +AD8041: FAQ
  • +AD8042: FAQ
  • +AD8045: FAQ
  • +AD8051: FAQ
  • +AD8074: FAQ
  • +AD8075: FAQ
  • +AD811: FAQ
  • +AD8128: FAQ
  • +AD8129: FAQ
  • +AD8130: FAQ
  • +AD8134: FAQ
  • +AD8145: FAQ
  • +AD8321: FAQ
  • +AD8328: FAQ
  • +AD8380: FAQ
  • +AD8381: FAQ
  • +AD8460: FAQ
  • +AD846: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9631: FAQ
  • +AD9776: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9882: FAQ
  • +AD9910: FAQ
  • +AD9911: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +ADA4302-4: FAQ
  • +ADA4355: FAQ
  • +ADA4411: FAQ
  • +ADA4853-2: FAQ
  • +ADAU1381: FAQ
  • +ADAU1461: FAQ
  • +ADAU1701: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADCMP580BCPZ-RL7: FAQ
  • +ADE5569: FAQ
  • +ADE7752: FAQ
  • +ADE7753: FAQ
  • +ADE7754: FAQ
  • +ADE7756: FAQ
  • +ADE7757: FAQ
  • +ADE7758: FAQ
  • +ADE7761: FAQ
  • +ADE7763: FAQ
  • +ADE7816: FAQ
  • +ADE7854: FAQ
  • +ADE7858: FAQ
  • +ADE7868: FAQ
  • +ADE7878: FAQ
  • +ADE7880: FAQ
  • +ADE7953: FAQ
  • +ADE7978: FAQ
  • +ADE9078: FAQ
  • +ADE9113: FAQ
  • +ADE9430: FAQ
  • +ADF4360: FAQ
  • +ADF5584: FAQ
  • +ADF7001: FAQ
  • +ADF7012: FAQ
  • +ADF7020: FAQ
  • +ADF7021-N: FAQ
  • +ADF7021-V: FAQ
  • +ADF7023: FAQ
  • +ADF7242: FAQ
  • +ADF7902: FAQ
  • +ADG201: FAQ
  • ADG324x Level Translation: high to low
  • +ADG623: FAQ
  • +ADIN6310: FAQ
  • +ADIS16204: FAQ
  • +ADIS16300: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16480: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADISIMPLL: FAQ
  • +ADISUSB: FAQ
  • +ADL5317: FAQ
  • +ADM1030: FAQ
  • +ADM1031: FAQ
  • +ADM1060: FAQ
  • +ADM1062: FAQ
  • +ADM1064: FAQ
  • +ADM1066: FAQ
  • +ADM1068: FAQ
  • +ADM1069: FAQ
  • +ADM1166: FAQ
  • +ADM1171: FAQ
  • +ADM1175: FAQ
  • +ADM1186: FAQ
  • +ADM3307: FAQ
  • +ADM869L: FAQ
  • +ADMC300: FAQ
  • +ADMTV315: FAQ
  • +ADMV4420: FAQ
  • +ADN2892: FAQ
  • +ADP1047: FAQ
  • +ADP1048: FAQ
  • +ADP195: FAQ
  • +ADP198: FAQ
  • +ADP3040: FAQ
  • +ADP3302: FAQ
  • +ADP3623: FAQ
  • +ADP3624: FAQ
  • +ADP5046: FAQ
  • +ADPA1112: FAQ
  • +ADPA9007: FAQ
  • +ADR125: FAQ
  • +ADRF5162: FAQ
  • +ADRF5700: FAQ
  • +ADRF6515: FAQ
  • +ADRV9002: FAQ
  • +ADRV9003: FAQ
  • +ADRV9026: FAQ
  • +ADRV9361-Z7035: FAQ
  • +ADRV9361: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • +ADSP-21365: FAQ
  • +ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +ADSP-BF533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF701: FAQ
  • +ADSP-CM408F: FAQ
  • +ADSP-TS001: FAQ
  • +ADT70: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +ADUC7020: FAQ
  • +ADUC7021: FAQ
  • +ADUC7023: FAQ
  • +ADUC7024: FAQ
  • +ADUC7026: FAQ
  • +ADUC7033: FAQ
  • +ADUC7060: FAQ
  • +ADUC7061: FAQ
  • +ADUC7120: FAQ
  • +ADUC7122: FAQ
  • +ADUC7126: FAQ
  • +ADUC7128: FAQ
  • +ADUC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADUC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADUC836: FAQ
  • +ADUC841: FAQ
  • +ADUC842: FAQ
  • +ADUC843: FAQ
  • +ADUC845: FAQ
  • +ADUC847: FAQ
  • +ADUC848: FAQ
  • +ADUCM360: FAQ
  • +ADUCM361: FAQ
  • +ADUCM362: FAQ
  • +ADUCM4050: FAQ
  • +ADUCM410: FAQ
  • +ADUCRF101: FAQ
  • +ADV7202: FAQ
  • +ADXL358: FAQ
  • +ADXL365: FAQ
  • +CABLE-PH04: FAQ
  • +CN0196: FAQ
  • +CN0287: FAQ
  • +CN0303: FAQ
  • +DC1075B-B: FAQ
  • +DC1854A: FAQ
  • +DC2039A: FAQ
  • +DC2046A-B: FAQ
  • +DC2393A: FAQ
  • +DC2465A: FAQ
  • +DC2617A: FAQ
  • +DC9000A: FAQ
  • +DC9018A-C: FAQ
  • +DC9021B: FAQ
  • +DC9022B: FAQ
  • +DS1010B UNTESTED RAW DIE: FAQ
  • +DS1181LE+: FAQ
  • DS1225AB-150: FAQ
  • +DS1225AB-150IND+: FAQ
  • +DS1225AD-200IND: FAQ
  • +DS1230Y-70IND+: FAQ
  • +DS1230Y: FAQ
  • +DS1235A: FAQ
  • +DS1236 UNTESTED UNLASERED DIE: FAQ
  • +DS1267-010: FAQ
  • +DS1267-10 UNTESTED RAW DIE: FAQ
  • +DS1270Y-70#: FAQ
  • +DS1270Y-70IND#: FAQ
  • +DS1312+: FAQ
  • +DS1402 BUTTON TO RJ11 PLUG CABLE: FAQ
  • +DS1402-RP8+: FAQ
  • +DS1402D-DR8+: FAQ
  • +DS1410E: FAQ
  • +DS1644-120: FAQ
  • +DS1669N-010: FAQ
  • +DS1821C+: FAQ
  • +DS1856B-020+: FAQ
  • +DS1856M: FAQ
  • +DS1859: FAQ
  • +DS1875K#: FAQ
  • +DS1904L-F5#: FAQ
  • +DS1920-F5+: FAQ
  • +DS1921: FAQ
  • +DS1922: FAQ
  • +DS1954: FAQ
  • +DS1961S: FAQ
  • +DS1963S: FAQ
  • +DS1971-F5+: FAQ
  • +DS1973-F3+: FAQ
  • +DS1977-F5#: FAQ
  • +DS1990A-019-F5A#CB: FAQ
  • +DS1990A-F3+: FAQ
  • +DS1990A-F5+: FAQ
  • +DS1991: FAQ
  • +DS1993: FAQ
  • +DS21554: FAQ
  • +DS2155DK: FAQ
  • +DS2155LNC2+: FAQ
  • +DS2482S-100+: FAQ
  • DS2482S-800+T&R: FAQ
  • +DS2483: FAQ
  • DS2490: FAQ
  • +DS2490S+: FAQ
  • +DS2506: FAQ
  • +DS26502DK: FAQ
  • +DS26502L+: FAQ
  • +DS26504: FAQ
  • +DS26504L+: FAQ
  • DS26514: FAQ
  • +DS26514GN+: FAQ
  • +DS26518DK: FAQ
  • +DS26518G+: FAQ
  • +DS26518GN+: FAQ
  • +DS26521L+: FAQ
  • +DS28CN01: FAQ
  • +DS28E01: FAQ
  • +DS28E04S-100+: FAQ
  • +DS28E11P+: FAQ
  • +DS3150TN+: FAQ
  • +DS3177+: FAQ
  • +DS34S132: FAQ
  • +DS34T101GN+: FAQ
  • +DS34T104: FAQ
  • +DS34T108GN+: FAQ
  • +DS3911: FAQ
  • +DS3935VGTL+: FAQ
  • +DS4100H+: FAQ
  • +DS4125: FAQ
  • DS4830A: FAQ
  • +DS4830AEVKIT: FAQ
  • +DS4830AT+: FAQ
  • DS75S-C1+T&R: FAQ
  • +DS80C320: FAQ
  • +DS80C323-ECD+: FAQ
  • +DS80C400-KIT: FAQ
  • +DS89C430-ENL+: FAQ
  • DS89C430: FAQ
  • +DS89C450-ENG+: FAQ
  • +DS89C450-QNG+: FAQ
  • +DS9034PC+: FAQ
  • +DS9034PCX+: FAQ
  • +DS9072: FAQ
  • +DS9090EVKIT#: FAQ
  • +DS9092+: FAQ
  • +DS9092L+: FAQ
  • +DS9092L: FAQ
  • +DS9093S+: FAQ
  • +DS9097U-009#: FAQ
  • +DS9097U-E25: FAQ
  • +DS9097U-S09#: FAQ
  • +DS9107+: FAQ
  • +DS9120P+: FAQ
  • +DS91230: FAQ
  • +DS9481P-300#: FAQ
  • +DS9490B#: FAQ
  • +DS9490B: FAQ
  • +DS9490R#: FAQ
  • +DSQ2FL1-J00+T: FAQ
  • +EV1HMC994APM5: FAQ
  • +EVAL-CN0566-RPIZ: FAQ
  • +EVAL-HCRWATCH4Z: FAQ
  • +EVAL-PRAOPAMP: FAQ
  • HMC-T2100: FAQ
  • +HMC1087: FAQ
  • +HMC1114: FAQ
  • +HMC342G: FAQ
  • +HMC518: FAQ
  • +HMC590: FAQ
  • +HMC6000: FAQ
  • +HMC605LP3E: FAQ
  • +HMC624: FAQ
  • +HMC6300G: FAQ
  • +HMC757: FAQ
  • +HMC852: FAQ
  • +HMC874: FAQ
  • +HMC930A: FAQ
  • +HMC994A: FAQ
  • +HSC-ADC-EVALB-DC: FAQ
  • HSC-ADC-EVALC: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +HSC_EVALBOARD: FAQ
  • +IA188EBPLC84IR2: FAQ
  • +IC0400C778BF+LTB: FAQ
  • +LM75BIMM-3+: FAQ
  • +LT1017: FAQ
  • +LT1161: FAQ
  • +LT1640A: FAQ
  • +LT4256-2: FAQ
  • +LT4293: FAQ
  • +LT4322: FAQ
  • +LTC2937: FAQ
  • +LTC2954: FAQ
  • +LTC2984: FAQ
  • +LTC2992: FAQ
  • +LTC3310: FAQ
  • +LTC4162: FAQ
  • +LTC4231: FAQ
  • +LTC4267-1: FAQ
  • +LTC4286: FAQ
  • +LTC4292: FAQ
  • +LTC4359: FAQ
  • +LTC4364: FAQ
  • +LTC4366: FAQ
  • +LTC4370: FAQ
  • +LTC4418: FAQ
  • +LTC4421: FAQ
  • +LTC6957-1: FAQ
  • +LTC7000: FAQ
  • +LTC9101-1: FAQ
  • +LTC9101-3: FAQ
  • +LTC9111: FAQ
  • +LTM2987: FAQ
  • +LTM4654: FAQ
  • +LTM4739: FAQ
  • +LTP5900-WHM: FAQ
  • +LTP5902-WHM: FAQ
  • +LTP8802: FAQ
  • +LTpowerCAD: FAQ
  • +LTSPICE: FAQ
  • +MAX-ECG-MONITOR: FAQ
  • +MAX-HEALTH-BAND: FAQ
  • +MAX-HEALTHBAND: FAQ
  • +MAX038CWP+_T1: FAQ
  • +MAX104CHC: FAQ
  • MAX13256: FAQ
  • +MAX13256ATB+: FAQ
  • +MAX14529E: FAQ
  • +MAX14626ETT+T: FAQ
  • +MAX14648: FAQ
  • MAX1464: FAQ
  • +MAX1464EVKIT: FAQ
  • +MAX14655: FAQ
  • +MAX14672ETB+: FAQ
  • +MAX14699EWC+: FAQ
  • +MAX14713EWL+: FAQ
  • +MAX14714EWL+: FAQ
  • +MAX14721ATP+: FAQ
  • +MAX14723ATP+: FAQ
  • MAX1472: FAQ
  • +MAX1472AKA+T: FAQ
  • +MAX14738EWT+T: FAQ
  • +MAX1479ATE+: FAQ
  • MAX14870: FAQ
  • +MAX14870ETC+: FAQ
  • +MAX14871EVKIT#: FAQ
  • MAX14874: FAQ
  • +MAX14874ETC+: FAQ
  • +MAX15068ATP+: FAQ
  • +MAX15090BEWI+: FAQ
  • +MAX15096AEWE+T: FAQ
  • MAX15096AGWE+: FAQ
  • +MAX15096AGWE+T: FAQ
  • +MAX15162AATE+: FAQ
  • +MAX15162AATG+: FAQ
  • +MAX15500: FAQ
  • +MAX16025TE+: FAQ
  • +MAX16028TP+: FAQ
  • +MAX16029: FAQ
  • MAX16046: FAQ
  • +MAX16046ACB+: FAQ
  • +MAX16046EVKIT+: FAQ
  • +MAX16050ETI+: FAQ
  • +MAX16065: FAQ
  • +MAX16084_XS22B+_A1: FAQ
  • +MAX16122AWT+: FAQ
  • +MAX16126TCA/V+: FAQ
  • +MAX16126_TCA/V+_A1: FAQ
  • +MAX16127TC/V+: FAQ
  • MAX16141/V+: FAQ
  • +MAX16141/V+T: FAQ
  • MAX16141AAAF/VY+: FAQ
  • +MAX16141AAAF/VY+T: FAQ
  • +MAX16141ATD+: FAQ
  • +MAX16141EVKIT#: FAQ
  • +MAX16141_AAF/V+_A1: FAQ
  • +MAX16165: FAQ
  • +MAX16545BGPF+T: FAQ
  • +MAX16550AGPN+: FAQ
  • +MAX16550GPN+T: FAQ
  • MAX16602GGN+: FAQ
  • +MAX16602GGN+T: FAQ
  • +MAX16946: FAQ
  • +MAX17523ATE+: FAQ
  • +MAX17525ATP+: FAQ
  • +MAX17526AATP+: FAQ
  • +MAX17561AUD+: FAQ
  • +MAX17563AUD+: FAQ
  • +MAX17600ASA+: FAQ
  • +MAX17601ASA+: FAQ
  • +MAX17606: FAQ
  • MAX17608: FAQ
  • +MAX17608ATC+: FAQ
  • +MAX17609: FAQ
  • +MAX17612AATB+: FAQ
  • +MAX17613AATP+: FAQ
  • +MAX17613A_TP+_A1: FAQ
  • +MAX17613BATP+: FAQ
  • +MAX17616A: FAQ
  • +MAX20323AENC+: FAQ
  • +MAX20323CENC+T: FAQ
  • +MAX20323DENC+T: FAQ
  • +MAX20328AEWA+: FAQ
  • +MAX20330AEWA+: FAQ
  • +MAX20331AEWL+: FAQ
  • +MAX21000+TWCHS: FAQ
  • +MAX21001/V+: FAQ
  • +MAX2150ETI+: FAQ
  • +MAX22200ETJ+: FAQ
  • +MAX22201: FAQ
  • +MAX22256: FAQ
  • +MAX2242: FAQ
  • +MAX235CPG+G36: FAQ
  • +MAX235MDG/HR: FAQ
  • +MAX253ESA+: FAQ
  • MAX256: FAQ
  • +MAX256ASA+: FAQ
  • +MAX2654EXT+: FAQ
  • +MAX274A: FAQ
  • +MAX274EVKIT-DIP+: FAQ
  • MAX28200EWC+T: FAQ
  • +MAX28200EWC+TC02: FAQ
  • MAX2828: FAQ
  • MAX2828ETN+: FAQ
  • +MAX2828ETN+T: FAQ
  • +MAX2829ETN+: FAQ
  • MAX2830: FAQ
  • MAX2830ETM+: FAQ
  • +MAX2830ETM+T: FAQ
  • MAX2831: FAQ
  • +MAX2831EVKIT: FAQ
  • +MAX2837ETM+: FAQ
  • +MAX2837EVKIT+: FAQ
  • +MAX2850: FAQ
  • +MAX2851ITK+: FAQ
  • +MAX2900ETI+: FAQ
  • +MAX291: FAQ
  • +MAX2990ECB+: FAQ
  • +MAX2992: FAQ
  • +MAX3111ECWI: FAQ
  • +MAX31740ATA+: FAQ
  • MAX31760AEE+: FAQ
  • +MAX31760AEE+T: FAQ
  • +MAX31785: FAQ
  • +MAX31785AETL+T: FAQ
  • MAX31790: FAQ
  • +MAX31790ATI+T: FAQ
  • +MAX31856MUD+: FAQ
  • +MAX32510: FAQ
  • +MAX32520/W+JU: FAQ
  • +MAX32520ATJJ/V+: FAQ
  • +MAX32550: FAQ
  • +MAX32552-LCJ+: FAQ
  • MAX32552: FAQ
  • +MAX32555/B+: FAQ
  • MAX32555: FAQ
  • +MAX32558: FAQ
  • +MAX32560: FAQ
  • +MAX32590-LNS+: FAQ
  • +MAX32620-EVKIT#: FAQ
  • +MAX32620-EVKIT: FAQ
  • +MAX32620FTHR#: FAQ
  • MAX32620FTHR: FAQ
  • +MAX32620ICQ+: FAQ
  • +MAX32620IWG+T: FAQ
  • +MAX32621-EVKIT#: FAQ
  • +MAX32621IWG+T: FAQ
  • +MAX32625-EVKIT#: FAQ
  • +MAX32625-EVKIT: FAQ
  • MAX32625: FAQ
  • +MAX32625ITK+: FAQ
  • +MAX32625MBED#: FAQ
  • +MAX32625MBED: FAQ
  • +MAX32625NEXPAQ: FAQ
  • +MAX32625PICO#: FAQ
  • +MAX32626-EVKIT#: FAQ
  • +MAX32626-EVKIT: FAQ
  • +MAX32626: FAQ
  • +MAX32630-EVKIT#: FAQ
  • +MAX32630FTHR#: FAQ
  • MAX32630FTHR: FAQ
  • +MAX32630ICQ+: FAQ
  • MAX32630IWG+: FAQ
  • +MAX32630IWG+T: FAQ
  • +MAX32631-EVKIT#: FAQ
  • MAX32631: FAQ
  • +MAX32631ICQ+: FAQ
  • +MAX32632: FAQ
  • +MAX32650-EVKIT#: FAQ
  • +MAX32650EVKIT: FAQ
  • +MAX32650GCE+: FAQ
  • +MAX32650GWQ+T: FAQ
  • MAX32651: FAQ
  • +MAX32651GCE+: FAQ
  • +MAX32652: FAQ
  • +MAX32655GWY+: FAQ
  • +MAX32660-EVKIT#: FAQ
  • -MAX32660-EVSYS#: FAQ
    • Do customer need to utilize the Eclipse IDE for Maxim's ARM-based Darwin microcontrollers?
    • Does Maxim have a µC-IDE for Darwin µC running on Linux?
    • Does the MAX32660-EVSYS contain a socket for the MAX32660?
    • Does the MAX32660-EVSYS include a MAX32625PICO board?
    • Is there a Bluetooth BLE radio on the MAX32660-EVSYS?
    • Is there a Keil Device Family Pack (DFP) for the MAX32660?
    • What is the Eclipse error when debugging: error (193)?
    • When I measure the Deep Sleep current on the MAX32660, I measure higher than the datasheet value. How can I verify the datasheet value?
    • Why do I have a MAX32660EVSYS UART_ReadAsync callback error -9 in the example code?
    • Why does Eclipse give this error: "undefined reference to 'header file', 'function'"?
    • Why does my UART on a Darwin microcontroller fail for debugging?
  • MAX32660: FAQ
  • +MAX32660EVKIT: FAQ
  • +MAX32660GTG+T: FAQ
  • +MAX32660GTGBL+: FAQ
  • +MAX32660GTGLA+T: FAQ
  • +MAX32660GWE+: FAQ
  • +MAX32665EVKIT#: FAQ
  • +MAX32665GXMBT+T: FAQ
  • +MAX32666FTHR#: FAQ
  • +MAX32666GWP+: FAQ
  • MAX32666GWPBT+: FAQ
  • +MAX32666GWPBT+T: FAQ
  • +MAX32668GWPBL+: FAQ
  • +MAX32670GTL+: FAQ
  • +MAX3421: FAQ
  • +MAX34440ETLA1+: FAQ
  • +MAX34446ETL+T: FAQ
  • +MAX34451ETNA1+: FAQ
  • +MAX34451ETNA2+: FAQ
  • +MAX34451ETNA3+: FAQ
  • +MAX34461AA00+: FAQ
  • +MAX34463EXQA3+: FAQ
  • +MAX3600: FAQ
  • +MAX3601GTL+: FAQ
  • +MAX3634: FAQ
  • +MAX3711: FAQ
  • +MAX3735AE/D: FAQ
  • +MAX3735AETG+: FAQ
  • +MAX3736ETE+: FAQ
  • +MAX3738: FAQ
  • +MAX3740AETG+: FAQ
  • MAX3740AETG: FAQ
  • +MAX3747AEUB+: FAQ
  • +MAX3748HETE+: FAQ
  • +MAX3761: FAQ
  • MAX3869EHJ+: FAQ
  • +MAX3869EHJ+T: FAQ
  • +MAX40056EVKIT#: FAQ
  • +MAX40200ANS+: FAQ
  • MAX40200AUK+: FAQ
  • +MAX40200AUK+T: FAQ
  • MAX40203ANS+: FAQ
  • +MAX40203ANS+T: FAQ
  • +MAX40213: FAQ
  • +MAX4137: FAQ
  • +MAX41460EVKIT: FAQ
  • +MAX41460GUB+: FAQ
  • +MAX41461GUB+T: FAQ
  • +MAX41463GUB+: FAQ
  • +MAX4201EUK+: FAQ
  • +MAX4207: FAQ
  • +MAX4222EEE+: FAQ
  • +MAX4311EEE+: FAQ
  • +MAX4370: FAQ
  • +MAX4383EEE+: FAQ
  • +MAX4427MJA/883B: FAQ
  • +MAX4428ESA+: FAQ
  • +MAX44299: FAQ
  • +MAX4444ESE/GG8: FAQ
  • +MAX4550EVKIT: FAQ
  • +MAX4820ETP+: FAQ
  • +MAX4821: FAQ
  • +MAX4896ATP+: FAQ
  • +MAX4915AELT+: FAQ
  • +MAX5048CAUT+: FAQ
  • +MAX5859EXW-D: FAQ
  • +MAX5902AAEUT+: FAQ
  • +MAX5903AAETT+: FAQ
  • +MAX5921FESA+: FAQ
  • +MAX5933AESA+: FAQ
  • +MAX5943AEEE+: FAQ
  • +MAX5947BESA: FAQ
  • +MAX5954AETX+: FAQ
  • +MAX5954LETX+: FAQ
  • +MAX5965A: FAQ
  • +MAX5969AETB+: FAQ
  • +MAX5969BETB+: FAQ
  • +MAX5969BEVKIT+: FAQ
  • +MAX5971AETI+: FAQ
  • +MAX5971BETI+: FAQ
  • +MAX5974AATE+T: FAQ
  • +MAX5974CETE+: FAQ
  • MAX5974D: FAQ
  • +MAX5974DATE+: FAQ
  • +MAX5974EETE+: FAQ
  • +MAX5977AETP+: FAQ
  • MAX5980: FAQ
  • +MAX5980AGTJ+: FAQ
  • +MAX5988A: FAQ
  • +MAX5991AETP+: FAQ
  • +MAX5995AATE+: FAQ
  • +MAX5995AETE+T: FAQ
  • +MAX5995BATE+: FAQ
  • +MAX5995CETE+: FAQ
  • +MAX6495: FAQ
  • +MAX6496ATA/V+: FAQ
  • +MAX6615AEE+: FAQ
  • +MAX6639FAEE: FAQ
  • +MAX6641: FAQ
  • +MAX6643LBBAEE+: FAQ
  • MAX6650: FAQ
  • +MAX6650EUB+: FAQ
  • +MAX6653AEE+: FAQ
  • +MAX6682MUA+T: FAQ
  • +MAX6684ESA+: FAQ
  • +MAX6816: FAQ
  • +MAX6839XSD2+: FAQ
  • +MAX6895AALT+: FAQ
  • +MAX6895AAZT/V+T: FAQ
  • +MAX7030HATJ+: FAQ
  • +MAX7032: FAQ
  • MAX7037: FAQ
  • +MAX7037EGL+T: FAQ
  • +MAX7037EVKIT#: FAQ
  • +MAX7461EUK+: FAQ
  • +MAX7474EAE+_T1: FAQ
  • +MAX77729XEWN+: FAQ
  • +MAX77823EWZ+: FAQ
  • +MAX77859AEWO+: FAQ
  • +MAX77932BEWO+: FAQ
  • +MAX77932EWO+T: FAQ
  • +MAX77972: FAQ
  • +MAX78000EXG+: FAQ
  • +MAX78000FTHR: FAQ
  • +MAX78700: FAQ
  • +MAX8535: FAQ
  • +MAX8790AETP+: FAQ
  • +MAX8804: FAQ
  • +MAX881: FAQ
  • +MAX8902: FAQ
  • +MAX8903: FAQ
  • +MAX9272: FAQ
  • +MAX9295AGTJ/V+: FAQ
  • +MAX9295EGTN/V+T: FAQ
  • +MAX9296AGTM/V+: FAQ
  • +MAX96716A: FAQ
  • +MAX96751: FAQ
  • +MAX96752: FAQ
  • +MAX96793: FAQ
  • +MAX98089ETN+: FAQ
  • +MAX98089EVKIT#WLP: FAQ
  • MAX98090: FAQ
  • +MAX98090AETL+T: FAQ
  • +MAX98090AEWJ+: FAQ
  • +MAX98090EVKIT#WLP: FAQ
  • +MAX98091: FAQ
  • +MAX98373: FAQ
  • +MAX9860ETG+: FAQ
  • MAX9867: FAQ
  • +MAX9867ETJ+: FAQ
  • +MAX9867EVKIT+: FAQ
  • MAX9880A: FAQ
  • +MAX9880AETM+: FAQ
  • +MAX9880AEVKIT#: FAQ
  • +MAX9947ETE+: FAQ
  • +MAXADCLITE+: FAQ
  • +MAXCOAX2STP-HSD#: FAQ
  • +MAXPOWERTOOL002#: FAQ
  • +MAXQ1741: FAQ
  • +MAXQ1743: FAQ
  • +MAXQ1744-DNS+: FAQ
  • +MAXQ617: FAQ
  • MAXQ7667: FAQ
  • +MAXQ7667AACM/V+: FAQ
  • +MAXQUSBJTAGOW-KIT#: FAQ
  • +MAXREFDES100#: FAQ
  • +MAXREFDES101 SOFTWARE FOR WINDOWS 10: FAQ
  • +MAXREFDES101#: FAQ
  • +MAXREFDES103#: FAQ
  • +MAXREFDES104#: FAQ
  • +MAXREFDES105#: FAQ
  • +MAXREFDES106: FAQ
  • +MAXREFDES117#: FAQ
  • +MAXREFDES132#: FAQ
  • +MAXREFDES145#: FAQ
  • +MAXREFDES150#: FAQ
  • +MAXREFDES16#: FAQ
  • +MAXREFDES165#: FAQ
  • +MAXREFDES212#: FAQ
  • +MAXREFDES220#: FAQ
  • +MAXREFDES280: FAQ
  • +MAXREFDES31#: FAQ
  • +MAXREFDES37#: FAQ
  • +MAXREFDES4#: FAQ
  • +MAXREFDES42#: FAQ
  • +MAXREFDES70#: FAQ
  • +MAXREFDES73#: FAQ
  • +MAXREFDES74#: FAQ
  • MAXREFDES74: FAQ
  • +MAXREFDES77#: FAQ
  • +MAXREFDES79#: FAQ
  • +MINIQUSB: FAQ
  • +NO PART NUMBER: FAQ
  • +NONE: FAQ
  • +OP07: FAQ
  • +OP27: FAQ
  • +OP37: FAQ
  • +OP90: FAQ
  • +PCB, MAX2850EVKIT+: FAQ
  • PD-1370: FAQ
  • +PD20-1-1210: FAQ
  • +PD28-3-1021-TMCL: FAQ
  • +PD42-1-1140-TMCL: FAQ
  • +PD42-1-1243-IOLINK: FAQ
  • +PD42-1-1370-TMCL: FAQ
  • +PD42-4-1370-TMCL: FAQ
  • +PD57-1-1076: FAQ
  • +PD57-1-1160-TMCL: FAQ
  • +PD57-1-1260-TMCL: FAQ
  • +PD57-1-1378-CANOPEN: FAQ
  • +PD57-2-1160-TMCL: FAQ
  • +PD60-3-1260-TMCL: FAQ
  • +PH-MODULES-TRINAMIC: FAQ
  • +QBL4208-100-04-025: FAQ
  • +QBL4208-41-04-006: FAQ
  • +QBL4208-61-04-013: FAQ
  • +QBL5704-116-04-042: FAQ
  • +QSH2818-32-07-006: FAQ
  • +QSH4218-41-10-035: FAQ
  • +REF02A: FAQ
  • +RS485: FAQ
  • +SC-USB-SPI: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2602: FAQ
  • +SSM2603: FAQ
  • +STM1E-SFP02: FAQ
  • +STM1E-SFP22: FAQ
  • +SW02: FAQ
  • +TEST: FAQ
  • +TMC USB-2-485: FAQ
  • +TMC2041-EVAL: FAQ
  • +TMC2041-LA: FAQ
  • +TMC2130-LA: FAQ
  • +TMC2208SILENTSTEPSTICK: FAQ
  • +TMC2209 SILENTSTEPSTICK: FAQ
  • +TMC2209-LA-T: FAQ
  • +TMC2226-BOB: FAQ
  • +TMC2240: FAQ
  • +TMC2590: FAQ
  • +TMC262C-LA: FAQ
  • +TMC2660C-PA-T: FAQ
  • TMC2660C-PA: FAQ
  • +TMC429-I: FAQ
  • +TMC4361A-LA: FAQ
  • +TMC457: FAQ
  • +TMC4671: FAQ
  • +TMC5031: FAQ
  • +TMC5041-LA: FAQ
  • +TMC5062-LA: FAQ
  • +TMC5072-LA: FAQ
  • +TMC5130-EVAL-KIT: FAQ
  • +TMC5130A-TA: FAQ
  • +TMC5160 SILENTSTEPSTICK: FAQ
  • +TMC5160-BOB: FAQ
  • +TMC5160-EVAL: FAQ
  • +TMC5160A-TA: FAQ
  • +TMC5240: FAQ
  • +TMC5272-EVAL-KIT: FAQ
  • +TMC6140-EVAL: FAQ
  • +TMC8462: FAQ
  • +TMCM-1043: FAQ
  • +TMCM-1070: FAQ
  • +TMCM-110-42-485: FAQ
  • +TMCM-1110 STEPROCKER: FAQ
  • +TMCM-1140-TMCL: FAQ
  • +TMCM-1160-TMCL: FAQ
  • +TMCM-1180-TMCL: FAQ
  • +TMCM-1240: FAQ
  • +TMCM-1260-CANOPEN: FAQ
  • +TMCM-1260-TMCL: FAQ
  • +TMCM-1270-CANOPEN: FAQ
  • +TMCM-1290: FAQ
  • +TMCM-142-IF-TMCL: FAQ
  • +TMCM-1630-2C: FAQ
  • +TMCM-1630-4U: FAQ
  • +TMCM-1633-CANOPEN: FAQ
  • +TMCM-1636-24V-CANOPEN: FAQ
  • +TMCM-1640: FAQ
  • +TMCM-1690: FAQ
  • +TMCM-310/SG: FAQ
  • +TMCM-3110-TMCL: FAQ
  • +TMCM-3212-TMCL: FAQ
  • +TMCM-3230-TMCL: FAQ
  • +TMCM-3314: FAQ
  • +TMCM-3351-TMCL: FAQ
  • +TMCM-6110: FAQ
  • +TMCM-6212-TMCL: FAQ
  • +TMCM-6214-CANOPEN: FAQ
  • +TMCM-6214-TMCL: FAQ
  • +TMCS: FAQ
  • +TRINAMIC MISC SERVICE: FAQ
  • +TRINAMIC PACKAGING SURCHARGE: FAQ
  • +USB-2-RTMI: FAQ
  • +USB2GPIO#: FAQ
  • +USB2PMB2#: FAQ
  • +VDSP-BLKFN-PC-FULL: FAQ
  • +VDSP-TS-PC-FULL: FAQ
  • +VISUALAUDIO: FAQ
  • +VT202: FAQ
  • +VT273SAFQ: FAQ
  • What does the "C01" denote in DS75S-C01+?
  • What should I do with unused I/O pins on the DS2482S?
  • +ZLP32300: FAQ
  • +_DS9093A: FAQ

When I measure the Deep Sleep current on the MAX32660, I measure higher than the datasheet value. How can I verify the datasheet value?

When measuring supply currents in the single digit microamperes (uA), it is important to inspect the board schematic for external loads including pull up resistors.  For example, if using the MAX32660-EVSYS, it is important to note that the DS28E05R+T is also being powered by the HDR_VIO net if R9 is populated.  In order to establish a base measurement, it is best if nothing is connected externally to the GPIOs and they should be configured as inputs with the internal pull-ups or pull-downs enabled.  Additional conditions are: RTC enabled and 96kB SRAM retained.

In summary:

  • RTC enabled
  • All GPIOs set to input with the pull-up enabled (pull-down yields similar results)
  • Nothing connected to the GPIOs externally
  • 96KB SRAM retained

If the GPIOs are set to Hi-Z, the current jumps to a higher value, so it is important to make sure the GPIOs are in a steady state.

 

Tags: deep sleep MAX32660-EVSYS# MAX32660 current KA-06665 MAX32660EVSYS Show More