Question: What is the recommended low power PMIC part number to be paired with the MAX32621/32631 Micros?
Answer:
- The MAX14690 is only available in WLP and it has a charger.
- The MAX14720 was used on the HSP (health system platform) is a great choice (but only available in WLP.)
- The MAX14750 is another very good PMIC Choice (but only available in WLP.)
- The MAX17270 and MAX3864x are lower IQ POLs and will be available in QFN packages