Question
On page 46 of datasheet, when ADF7021 communicates with SCM and use Standard
Transmit/Receive Data Interface mode, there is a diode in MISO port, what is it
used for?
Answer
This diode is used for unidirection protection.
1)ADuC Receive mode: in this mode,ADF7021 TxRxDATA pin send data to ADuC84x
MOSI pin.MISO must keep high to cut off diode to make sure MISO data does not
interrupt TxRxData.
2)ADuC Transmit mode: in this mode, ADF7021 xRxData pin receive ADuC84x
data.there is a pull up in TxRxData pin, when MISO send 0, diode current flows
and 0 is sent to TxRxData, if sending 1, diode cut off and pull up takes
TxRxData pin to high and realize input 1.