Question
Does the ADF7023 support spectrum inversion?
Answer
The ADF7023 will generate FSK or GFSK, where the –Fdev is equivalent to a 0,
and the +FDev is equivalent to a 1, or OOK where the 0 is off, the 1 is on. If
by frequency inversion you want the opposite mapping of FDev, then this would
have to be done by inverting the source data.
The Tx test modes we offer are Tx carrier, Tx Preamble or Tx PN9, or SPORT Mode
Tx will simply follow the DataTransmit pin.