Question
Is it possible to get the FPGA source code from HSC-ADC-EVALCZ High speed adc
evaluations boards for customer?
Answer
The FPGA design files are available at the following link:
ftp://ftp.analog.com/pub/HSSP_SW/fpga
For users interested in customizing our standard HSC-ADC-EVALCZ hardware and/or
our distributed FPGA capture code we do provide the full hardware BOM,
schematics, and FPGA source code upon request. ADC model specific
HSC-ADC-EVALCZ FPGA source code is typically posted to our public FTP site at
ftp://ftp.analog.com/pub/HSSP_SW/fpga/. The Virtex4 can also be accessed for
programming directly via JTAG header J10 using standard ISE development tools
available from Xilinx.
There are also several discussions on modifying the FPGA source code at the
Engineer Zone, if he searches for "HSC-ADC-EVALCZ" & "FPGA" , you should be
able to locate those discussions.