Question
We are seeking a sensor similar to the ADIS16448, but without the pressure
sensor and housing, to allow for higher integration. The module must be still
functional after an acceleration of approximately 30000g. The technical data
should be at least as good as the ADIS16448
Answer
As far as I am aware, the actual packaging/housing of our ADIS parts
contributes to the overall performance of the parts. If it were to be removed,
the specifications stated in the datasheet would not apply.
In terms of shock survival, the ADIS16448 is rated up to 2000g.
There are 6 degree of freedom parts with similar specifications:
ADIS16485
ADIS16445