Question
I use in a project the ADM1062 for monitoring some voltages. I want to use the
ADM1062 only for analog digital conversion from the inputs VX1-5, VP1-4, VH an
internal temperature sensor without averaging.
I don't want to use the EEPROM for configuration. I want to initialize the
ADM1062 every start up over the SMBus. Can you tell me which register I have to
write for the configuration to read the ADC Value Register
continuously?
Answer
Yes, this is possible. There are several ADC registers to configure and then do
the readback, they’re documented in the AN-698, and there’s also another apps
note, AN-897, dealing with how to setup and configure and use the ADC as well.