Question
I need only left channel of SPDIF audio and microphone in same time. It is
possible to configure codec to work in this way (analogue audio – MIC and left
or right channel from digital input )?
Answer
Yes, you can connect both one analog and one digital input channel to the
ADAU1761 and process both of them together. If you are using the serial digital
input port, you should ensure that the serial port is synchronized with the
master clock that is sent to the codec.