Where can I find an CRC API example for the MAX32630/31/32?
The examples are downloaded using the ARMCortexToolchain installer. You can easily choose to download only the product specific resources/firmware. Once you finish the installation, look in the installation location you specified. The folder named "Firmware" contains the SDK API and examples. So for the MAX32630/31/32, the CRC example is located in <install dir>\Firmware\MAX3263X\Applications\EvKitExamples\CRC\.