The maximum clock speed supported by the present series of low power microcontrollers is 96MHz. This is an optimum value because it is the integral multiple of the speed of the USB protocol which is 48MHz. The future series of microcontrollers will support up to 120MHz.