This webinar is an overview of the EMC tests ADI subjects its digital isolators to, why these tests are preformed and the performance of current and previous...
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
      1. First, the quote of the week: " The best measure of a man's honesty isn't his income tax return. It's the zero adjust on his bathroom scale " - Unknown...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: White Coats and Multi-Coloured Pens Ready to put...
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
    What happens when your system needs to talk across noisy or high-voltage boundaries? Isolation steps in. In a previous blog post, we discussed the fundamentals...

     

    Understanding Safe Failure Fraction: Can There Be Multiple Values?

    I discuss various aspects of the SFF (safe failure fraction) —whether it applies to an integrated circuit —and whether an integrated circuit can have more...
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
Other Products (EN)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other Products (EN)
Other Products (EN)
Documents What are the trade-offs between power consumption and conversion speed in the MAX1464?
  • Forums
  • FAQs/ Docs
  • Members
  • Tags
  • Cancel
  • +Documents
  • +AD10200: FAQ
  • +AD8436: FAQ
  • 3B01: the connection between the 26-pin and 16 channel.
  • 442 - I cannot find the datasheet for the 442 (old OPAMP Module)
  • 751: old datasheet
  • Ac coupling Vs Dc coupling
  • AC1307E Power Supply input range
  • AD-MSDPD-EVB: Eval Board Datasheet
  • ADATE304 Force Voltage
  • ADATE318: What supply voltage do I use for VDD_THERM?
  • ADMP401 startup
  • ADMP441 output format
  • +ADN2531: Can output be configured as current source?
  • ADN2685: could you send the final datasheet?
  • +ADN2814: FAQ
  • +ADN2816: FAQ
  • ADN2817 error correction
  • ADN2820: Optical fiber communication
  • +ADN2830: FAQ
  • +ADN2871: Differential drive circuit for driving a VCSEL Laser diode.
  • +ADN2872: Is it possible to use 2 laser drivers in parallel to have the modulation current of 130 mA?   
  • ADN2873: Minimum differential signal between the DATAP and DATAN
  • ADN2880: MAX leakage current specification of ADN2880 input
  • +ADN2882 Evaluation Board
  • +ADN4600: FAQ
  • +ADN469xE: FAQ
  • +ADN8831: FAQ
  • ADN8834: Evaluation board difference
  • AN-695 Q&A
  • Aqueous washing of ADI parts?
  • Baking BGA in Tray or trays
  • Baking of parts in a Reel
  • Can ADN4604 do single ended 75Ohm input and output?
  • Can I connect one input to multiple outputs?
  • datasheet 2B35
  • Digital programmable power with 1.8V logic to Vout = 5V
  • Does changing the crosspoint connectivity affect the state of previously configured connections?
  • doubling ADN8810 Iout configuration query (SR#: 1202803)
  • EVAL-AD8436 evaluation board operation with single supply
  • Failure probability for AD8468
  • How can I order Linear Circuit Design Handbook?
  • Maximum Recommended PMU Load Capacitance
  • MTBF-reliability data
  • Package general: What is the pin pitch of LFCSP package?
  • Package: 10 ld Ceramic Flat Package footprints
  • paste mask recommendation
  • PFC controller + LED driver in one package
  • Replacement for PMI119-883
  • RoHS compliant status E
  • RTI-850 RTI products
  • Shelf life for Analog parts
  • Shelf life of drypack used to ship Moisture/Reflow Sensitive Surface Mount Devices
  • The unit of MTTF data on ADI web site
  • transistor counts for a processor to calculate the MTBF
  • unused inputs or outputs?
  • What data rates or range of data rates are supported?
  • What data rates protocols are supported?
  • Where can I find e-book versions on your seminar books to download?
  • which register we can read to know the status of HD
  • Why the Analog Input Current from ?10mA to 10 mA was limited.
  • +#N/A: FAQ
  • +--: FAQ
  • +1-WIRE + I2C MULTI-DEVICE PROGRAMMER: FAQ
  • +125932-HMC675LP3E: FAQ
  • 1s74: FAQ
  • +310: FAQ
  • +73M1X22: FAQ
  • +73S8010C-ILR/F: FAQ
  • +78P2351-IGT: FAQ
  • +78Q2123/F: FAQ
  • +78Q8392LA03-CHR/F: FAQ
  • +940: FAQ
  • +AD-CELLPACKBM-SL: FAQ
  • +AD-GMSL522-SL: FAQ
  • AD1835: FAQ
  • +AD1835A: FAQ
  • AD1836: FAQ
  • +AD1836A: FAQ
  • +AD1845: FAQ
  • +AD1862: FAQ
  • +AD1881A: FAQ
  • +AD1937: FAQ
  • +AD1938: FAQ
  • +AD1939: FAQ
  • +AD1970: FAQ
  • AD1981: FAQ
  • +AD1981B: FAQ
  • +AD1986: FAQ
  • +AD1992: FAQ
  • +AD22151: FAQ
  • +AD22282-A-R2: FAQ
  • +AD22290: FAQ
  • +AD4080: FAQ
  • +AD506: FAQ
  • +AD53500: FAQ
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD598JRZ: FAQ
  • +AD630: FAQ
  • +AD644: FAQ
  • +AD6635: FAQ
  • +AD671: FAQ
  • +AD7124: FAQ
  • +AD7280: FAQ
  • +AD73311: FAQ
  • +AD73311L: FAQ
  • AD73322: FAQ
  • +AD73322L: FAQ
  • +AD74111: FAQ
  • +AD7503: FAQ
  • +AD7546: FAQ
  • +AD7725: FAQ
  • +AD7756: FAQ
  • +AD8036: FAQ
  • +AD8041: FAQ
  • +AD8042: FAQ
  • +AD8045: FAQ
  • +AD8051: FAQ
  • +AD8074: FAQ
  • +AD8075: FAQ
  • +AD811: FAQ
  • +AD8128: FAQ
  • +AD8129: FAQ
  • +AD8130: FAQ
  • +AD8134: FAQ
  • +AD8145: FAQ
  • +AD8321: FAQ
  • +AD8328: FAQ
  • +AD8380: FAQ
  • +AD8381: FAQ
  • +AD8460: FAQ
  • +AD846: FAQ
  • +AD9102: FAQ
  • +AD9106: FAQ
  • +AD9631: FAQ
  • +AD9776: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9882: FAQ
  • +AD9910: FAQ
  • +AD9911: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +ADA4302-4: FAQ
  • +ADA4355: FAQ
  • +ADA4411: FAQ
  • +ADA4853-2: FAQ
  • +ADAU1381: FAQ
  • +ADAU1461: FAQ
  • +ADAU1701: FAQ
  • +ADAU1761: FAQ
  • +ADAU1772: FAQ
  • +ADCMP580BCPZ-RL7: FAQ
  • +ADE5569: FAQ
  • +ADE7752: FAQ
  • +ADE7753: FAQ
  • +ADE7754: FAQ
  • +ADE7756: FAQ
  • +ADE7757: FAQ
  • +ADE7758: FAQ
  • +ADE7761: FAQ
  • +ADE7763: FAQ
  • +ADE7816: FAQ
  • +ADE7854: FAQ
  • +ADE7858: FAQ
  • +ADE7868: FAQ
  • +ADE7878: FAQ
  • +ADE7880: FAQ
  • +ADE7953: FAQ
  • +ADE7978: FAQ
  • +ADE9078: FAQ
  • +ADE9113: FAQ
  • +ADE9430: FAQ
  • +ADF4360: FAQ
  • +ADF5584: FAQ
  • +ADF7001: FAQ
  • +ADF7012: FAQ
  • +ADF7020: FAQ
  • +ADF7021-N: FAQ
  • +ADF7021-V: FAQ
  • +ADF7023: FAQ
  • +ADF7242: FAQ
  • +ADF7902: FAQ
  • +ADG201: FAQ
  • ADG324x Level Translation: high to low
  • +ADG623: FAQ
  • +ADIN6310: FAQ
  • +ADIS16204: FAQ
  • +ADIS16300: FAQ
  • +ADIS16355: FAQ
  • +ADIS16364: FAQ
  • +ADIS16365: FAQ
  • +ADIS16375: FAQ
  • +ADIS16385: FAQ
  • +ADIS16400: FAQ
  • +ADIS16405: FAQ
  • +ADIS16407: FAQ
  • +ADIS16445: FAQ
  • +ADIS16448: FAQ
  • +ADIS16480: FAQ
  • +ADIS16485: FAQ
  • +ADIS16488: FAQ
  • +ADISIMPLL: FAQ
  • +ADISUSB: FAQ
  • +ADL5317: FAQ
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
  • +ADM1186: FAQ
  • +ADM3307: FAQ
  • +ADM869L: FAQ
  • +ADMC300: FAQ
  • +ADMTV315: FAQ
  • +ADMV4420: FAQ
  • +ADN2892: FAQ
  • +ADP1047: FAQ
  • +ADP1048: FAQ
  • +ADP195: FAQ
  • +ADP198: FAQ
  • +ADP3040: FAQ
  • +ADP3302: FAQ
  • +ADP3623: FAQ
  • +ADP3624: FAQ
  • +ADP5046: FAQ
  • +ADPA1112: FAQ
  • +ADPA9007: FAQ
  • +ADR125: FAQ
  • +ADRF5162: FAQ
  • +ADRF5700: FAQ
  • +ADRF6515: FAQ
  • +ADRV9002: FAQ
  • +ADRV9003: FAQ
  • +ADRV9026: FAQ
  • +ADRV9361: FAQ
  • +ADSP-21160M: FAQ
  • +ADSP-21363: FAQ
  • +ADSP-21365: FAQ
  • +ADSP-21368: FAQ
  • +ADSP-21369: FAQ
  • +ADSP-21469: FAQ
  • +ADSP-21489: FAQ
  • +ADSP-BF522: FAQ
  • +ADSP-BF531: FAQ
  • +ADSP-BF532: FAQ
  • +ADSP-BF533: FAQ
  • +ADSP-BF534: FAQ
  • +ADSP-BF535: FAQ
  • +ADSP-BF536: FAQ
  • +ADSP-BF537: FAQ
  • +ADSP-BF538F: FAQ
  • +ADSP-BF539: FAQ
  • +ADSP-BF542: FAQ
  • +ADSP-BF544: FAQ
  • +ADSP-BF561: FAQ
  • +ADSP-BF609: FAQ
  • +ADSP-BF701: FAQ
  • +ADSP-CM408F: FAQ
  • +ADSP-TS001: FAQ
  • +ADT70: FAQ
  • +ADT7460: FAQ
  • +ADT7461: FAQ
  • +ADUC7020: FAQ
  • +ADUC7021: FAQ
  • +ADUC7023: FAQ
  • +ADUC7024: FAQ
  • +ADUC7026: FAQ
  • +ADUC7033: FAQ
  • +ADUC7060: FAQ
  • +ADUC7061: FAQ
  • +ADUC7120: FAQ
  • +ADUC7122: FAQ
  • +ADUC7126: FAQ
  • +ADUC7128: FAQ
  • +ADUC812: FAQ
  • +ADUC814: FAQ
  • +ADUC816: FAQ
  • +ADUC824: FAQ
  • +ADUC831: FAQ
  • +ADUC832: FAQ
  • +ADUC834: FAQ
  • +ADUC836: FAQ
  • +ADUC841: FAQ
  • +ADUC842: FAQ
  • +ADUC843: FAQ
  • +ADUC845: FAQ
  • +ADUC847: FAQ
  • +ADUC848: FAQ
  • +ADUCM360: FAQ
  • +ADUCM361: FAQ
  • +ADUCM362: FAQ
  • +ADUCM4050: FAQ
  • +ADUCM410: FAQ
  • +ADUCRF101: FAQ
  • +ADV7202: FAQ
  • +ADXL358: FAQ
  • +ADXL365: FAQ
  • +CABLE-PH04: FAQ
  • +CN0196: FAQ
  • +CN0287: FAQ
  • +CN0303: FAQ
  • +DC1075B-B: FAQ
  • +DC1854A: FAQ
  • +DC2039A: FAQ
  • +DC2046A-B: FAQ
  • +DC2393A: FAQ
  • +DC2465A: FAQ
  • +DC2617A: FAQ
  • +DC9000A: FAQ
  • +DC9018A-C: FAQ
  • +DC9021B: FAQ
  • +DC9022B: FAQ
  • +DS1010B UNTESTED RAW DIE: FAQ
  • +DS1181LE+: FAQ
  • DS1225AB-150: FAQ
  • +DS1225AB-150IND+: FAQ
  • +DS1225AD-200IND: FAQ
  • +DS1230Y: FAQ
  • +DS1235A: FAQ
  • +DS1236 UNTESTED UNLASERED DIE: FAQ
  • +DS1267-010: FAQ
  • +DS1267-10 UNTESTED RAW DIE: FAQ
  • +DS1270Y-70#: FAQ
  • +DS1270Y-70IND#: FAQ
  • +DS1312+: FAQ
  • +DS1402 BUTTON TO RJ11 PLUG CABLE: FAQ
  • +DS1402-RP8+: FAQ
  • +DS1402D-DR8+: FAQ
  • +DS1410E: FAQ
  • +DS1644-120: FAQ
  • +DS1669N-010: FAQ
  • +DS1821C+: FAQ
  • +DS1856B-020+: FAQ
  • +DS1856M: FAQ
  • +DS1859: FAQ
  • +DS1875K#: FAQ
  • +DS1904L-F5#: FAQ
  • +DS1920-F5+: FAQ
  • +DS1921: FAQ
  • +DS1922: FAQ
  • +DS1954: FAQ
  • +DS1961S: FAQ
  • +DS1963S: FAQ
  • +DS1971-F5+: FAQ
  • +DS1973-F3+: FAQ
  • +DS1977-F5#: FAQ
  • +DS1990A-019-F5A#CB: FAQ
  • +DS1990A-F3+: FAQ
  • +DS1990A-F5+: FAQ
  • +DS1991: FAQ
  • +DS1993: FAQ
  • +DS21554: FAQ
  • +DS2155DK: FAQ
  • +DS2155LNC2+: FAQ
  • +DS2482S-100+: FAQ
  • DS2482S-800+T&R: FAQ
  • +DS2483: FAQ
  • DS2490: FAQ
  • +DS2490S+: FAQ
  • +DS2506: FAQ
  • +DS26502DK: FAQ
  • +DS26502L+: FAQ
  • +DS26504: FAQ
  • +DS26504L+: FAQ
  • DS26514: FAQ
  • +DS26514GN+: FAQ
  • +DS26518DK: FAQ
  • +DS26518G+: FAQ
  • +DS26518GN+: FAQ
  • +DS26521L+: FAQ
  • +DS28CN01: FAQ
  • +DS28E01: FAQ
  • +DS28E04S-100+: FAQ
  • +DS28E11P+: FAQ
  • +DS3150TN+: FAQ
  • +DS3177+: FAQ
  • +DS34S132: FAQ
  • +DS34T101GN+: FAQ
  • +DS34T104: FAQ
  • +DS34T108GN+: FAQ
  • +DS3911: FAQ
  • +DS3935VGTL+: FAQ
  • +DS4100H+: FAQ
  • +DS4125: FAQ
  • DS4830A: FAQ
  • +DS4830AEVKIT: FAQ
  • +DS4830AT+: FAQ
  • DS75S-C1+T&R: FAQ
  • +DS80C320: FAQ
  • +DS80C323-ECD+: FAQ
  • +DS80C400-KIT: FAQ
  • +DS89C430-ENL+: FAQ
  • DS89C430: FAQ
  • +DS89C450-ENG+: FAQ
  • +DS89C450-QNG+: FAQ
  • +DS9034PC+: FAQ
  • +DS9034PCX+: FAQ
  • +DS9072: FAQ
  • +DS9090EVKIT#: FAQ
  • +DS9092+: FAQ
  • +DS9092L+: FAQ
  • +DS9092L: FAQ
  • +DS9093S+: FAQ
  • +DS9097U-009#: FAQ
  • +DS9097U-E25: FAQ
  • +DS9097U-S09#: FAQ
  • +DS9107+: FAQ
  • +DS9120P+: FAQ
  • +DS91230: FAQ
  • +DS9481P-300#: FAQ
  • +DS9490B#: FAQ
  • +DS9490B: FAQ
  • +DS9490R#: FAQ
  • +DSQ2FL1-J00+T: FAQ
  • +EV1HMC994APM5: FAQ
  • +EVAL-CN0566-RPIZ: FAQ
  • +EVAL-HCRWATCH4Z: FAQ
  • +EVAL-PRAOPAMP: FAQ
  • HMC-T2100: FAQ
  • +HMC1087: FAQ
  • +HMC1114: FAQ
  • +HMC342G: FAQ
  • +HMC518: FAQ
  • +HMC590: FAQ
  • +HMC6000: FAQ
  • +HMC605LP3E: FAQ
  • +HMC624: FAQ
  • +HMC6300G: FAQ
  • +HMC757: FAQ
  • +HMC852: FAQ
  • +HMC874: FAQ
  • +HMC930A: FAQ
  • +HSC-ADC-EVALB-DC: FAQ
  • HSC-ADC-EVALC: FAQ
  • +HSC-ADC-EVALCZ: FAQ
  • +HSC_EVALBOARD: FAQ
  • +IA188EBPLC84IR2: FAQ
  • +IC0400C778BF+LTB: FAQ
  • +LM75BIMM-3+: FAQ
  • +LT1017: FAQ
  • +LT1161: FAQ
  • +LT1640A: FAQ
  • +LT4256-2: FAQ
  • +LT4293: FAQ
  • +LT4322: FAQ
  • +LTC2937: FAQ
  • +LTC2954: FAQ
  • +LTC2984: FAQ
  • +LTC2992: FAQ
  • +LTC3310: FAQ
  • +LTC4162: FAQ
  • +LTC4231: FAQ
  • +LTC4267-1: FAQ
  • +LTC4286: FAQ
  • +LTC4292: FAQ
  • +LTC4359: FAQ
  • +LTC4364: FAQ
  • +LTC4366: FAQ
  • +LTC4370: FAQ
  • +LTC4418: FAQ
  • +LTC4421: FAQ
  • +LTC6957-1: FAQ
  • +LTC7000: FAQ
  • +LTC9101-1: FAQ
  • +LTC9101-3: FAQ
  • +LTC9111: FAQ
  • +LTM2987: FAQ
  • +LTM4654: FAQ
  • +LTM4739: FAQ
  • +LTP5900-WHM: FAQ
  • +LTP5902-WHM: FAQ
  • +LTP8802: FAQ
  • +LTpowerCAD: FAQ
  • +LTSPICE: FAQ
  • +MAX-ECG-MONITOR: FAQ
  • +MAX-HEALTH-BAND: FAQ
  • +MAX-HEALTHBAND: FAQ
  • +MAX038CWP+_T1: FAQ
  • +MAX104CHC: FAQ
  • MAX13256: FAQ
  • +MAX13256ATB+: FAQ
  • +MAX14529E: FAQ
  • +MAX14626ETT+T: FAQ
  • +MAX14648: FAQ
  • MAX1464: FAQ
  • -MAX1464EVKIT: FAQ
    • Are there any programming examples available for the MAX1464?
    • Can I use the Control program in both 3-wire and 4-wire communication for the MAX1464?
    • Can I use the MAX1464 hardware debugger program in both 3-wire and 4-wire communication?
    • Can Partition-1 (user portion) of the MAX1464 flash memory be accessed by the CPU program?
    • Can the MAX1464 be used to measure the RTDs or K-type thermocouples?
    • Can the op amps on the MAX1464 be used as uncommitted op amps?
    • Can the second-order compensation algorithm built into the MAX1464 Control Program be used for real compensation in production?
    • Does the input impedance of the MAX1464 change with different PGA gain settings? How?
    • How can I switch the MAX1464 EV board from 3-wire to 4-wire communication, and vice versa?
    • How can the Control Program be used for the MAX1464?
    • How can the MAX1464 Hardware Debugger be used?
    • How do I program the MAX1464?
    • How is the conversion resolution affected by the changing conversion rate in the MAX1464?
    • How many input channels does the MAX1464 have?
    • I get 'file operation' failure error when launching the Control Program for the MAX1464. What is the problem?
    • Is it possible to call the MAX1464 DLL functions from Visual Basic?
    • Is the common-mode range specification the same for all PGA gain settings in the MAX1464?
    • Is the internal temperature sensor of the MAX1463 the same as on the MAX1464?
    • Is the MAX1464 temperature sensor output ratiometric to VDD?
    • MAX1464EVKIT Software OS Support
    • My setup is correct but cannot communicate with the MAX1464. What is the problem?
    • On what platform are the MAX1464 DLLs developed?
    • The 'DUT?' button on the Control Program window does not turn green when I start the program for the MAX1464. What is wrong?
    • Turning the potentiometers on the EV board does not change the input to the MAX1464. What is the problem?
    • What are the differences between 3-wire and 4-wire interfaces for the MAX1464?
    • What are the hardware differences between the MAX1463 and the MAX1464?
    • What are the register definition differences between MAX1463 and MAX1464?
    • What are the trade-offs between power consumption and conversion speed in the MAX1464?
    • What extent of programming can be realized with the available 4kB of flash memory for the MAX1464?
    • What input voltage range can the MAX1464 accommodate?
    • What instructions are available for the MAX1464 microprocessor?
    • What is an example application of the MAX1464 signal conditioner?
    • What is included in the MAX1464 evaluation kit?
    • What is the allowed common-mode voltage range for the INPx and INMx input voltages in the MAX1464?
    • What is the flash-memory capacity in the MAX1464?
    • What is the function of the partition-1 of the flash memory in the MAX1464?
    • What is the MAX1464's data-retention rating as a function of temperature?
    • What is the MAX1464?
    • What is the maximum supply voltage at which the MAX1464 can operate without damaging the part?
    • What is the relationship between ADC clock rates and power consumption in the MAX1464?
    • What is the sequence of events that take place to complete one ADC conversion for the MAX1464?
    • What should be the relationship between the output impedance of the sensor and input impedance of the MAX1464? How are they affecting each other?
    • What software tools are available to use with the MAX1464?
    • When starting an ADC cycle in the MAX1464, how long does it take before sampling starts?
    • When the MAX1464 ADC is sampling does it start with LSB or MSB?
    • With which Windows®︎ platform is the MAX1464 Hardware Debugger compatible?
    • With which Windows®︎ platforms are the MAX1464 DLLs compatible?
  • +MAX14655: FAQ
  • +MAX14672ETB+: FAQ
  • +MAX14699EWC+: FAQ
  • +MAX14713EWL+: FAQ
  • +MAX14714EWL+: FAQ
  • +MAX14721ATP+: FAQ
  • +MAX14723ATP+: FAQ
  • MAX1472: FAQ
  • +MAX1472AKA+T: FAQ
  • +MAX14738EWT+T: FAQ
  • +MAX1479ATE+: FAQ
  • MAX14870: FAQ
  • +MAX14870ETC+: FAQ
  • +MAX14871EVKIT#: FAQ
  • MAX14874: FAQ
  • +MAX14874ETC+: FAQ
  • +MAX15068ATP+: FAQ
  • +MAX15090BEWI+: FAQ
  • +MAX15096AEWE+T: FAQ
  • MAX15096AGWE+: FAQ
  • +MAX15096AGWE+T: FAQ
  • +MAX15162AATE+: FAQ
  • +MAX15162AATG+: FAQ
  • +MAX15500: FAQ
  • +MAX16025TE+: FAQ
  • +MAX16028TP+: FAQ
  • +MAX16029: FAQ
  • MAX16046: FAQ
  • +MAX16046ACB+: FAQ
  • +MAX16046EVKIT+: FAQ
  • +MAX16050ETI+: FAQ
  • +MAX16065: FAQ
  • +MAX16084_XS22B+_A1: FAQ
  • +MAX16122AWT+: FAQ
  • +MAX16126TCA/V+: FAQ
  • +MAX16126_TCA/V+_A1: FAQ
  • +MAX16127TC/V+: FAQ
  • MAX16141/V+: FAQ
  • +MAX16141/V+T: FAQ
  • MAX16141AAAF/VY+: FAQ
  • +MAX16141AAAF/VY+T: FAQ
  • +MAX16141ATD+: FAQ
  • +MAX16141EVKIT#: FAQ
  • +MAX16141_AAF/V+_A1: FAQ
  • +MAX16165: FAQ
  • +MAX16545BGPF+T: FAQ
  • +MAX16550AGPN+: FAQ
  • +MAX16550GPN+T: FAQ
  • MAX16602GGN+: FAQ
  • +MAX16602GGN+T: FAQ
  • +MAX16946: FAQ
  • +MAX17523ATE+: FAQ
  • +MAX17525ATP+: FAQ
  • +MAX17526AATP+: FAQ
  • +MAX17561AUD+: FAQ
  • +MAX17563AUD+: FAQ
  • +MAX17600ASA+: FAQ
  • +MAX17601ASA+: FAQ
  • +MAX17606: FAQ
  • MAX17608: FAQ
  • +MAX17608ATC+: FAQ
  • +MAX17609: FAQ
  • +MAX17612AATB+: FAQ
  • +MAX17613AATP+: FAQ
  • +MAX17613A_TP+_A1: FAQ
  • +MAX17613BATP+: FAQ
  • +MAX17616A: FAQ
  • +MAX20323AENC+: FAQ
  • +MAX20323CENC+T: FAQ
  • +MAX20323DENC+T: FAQ
  • +MAX20328AEWA+: FAQ
  • +MAX20330AEWA+: FAQ
  • +MAX20331AEWL+: FAQ
  • +MAX21000+TWCHS: FAQ
  • +MAX21001/V+: FAQ
  • +MAX2150ETI+: FAQ
  • +MAX22200ETJ+: FAQ
  • +MAX22201: FAQ
  • +MAX22256: FAQ
  • +MAX2242: FAQ
  • +MAX235CPG+G36: FAQ
  • +MAX235MDG/HR: FAQ
  • +MAX253ESA+: FAQ
  • MAX256: FAQ
  • +MAX256ASA+: FAQ
  • +MAX2654EXT+: FAQ
  • +MAX274A: FAQ
  • +MAX274EVKIT-DIP+: FAQ
  • MAX28200EWC+T: FAQ
  • +MAX28200EWC+TC02: FAQ
  • MAX2828: FAQ
  • MAX2828ETN+: FAQ
  • +MAX2828ETN+T: FAQ
  • +MAX2829ETN+: FAQ
  • MAX2830: FAQ
  • MAX2830ETM+: FAQ
  • +MAX2830ETM+T: FAQ
  • MAX2831: FAQ
  • +MAX2831EVKIT: FAQ
  • +MAX2837ETM+: FAQ
  • +MAX2837EVKIT+: FAQ
  • +MAX2850: FAQ
  • +MAX2851ITK+: FAQ
  • +MAX2900ETI+: FAQ
  • +MAX291: FAQ
  • +MAX2990ECB+: FAQ
  • +MAX2992: FAQ
  • +MAX3111ECWI: FAQ
  • +MAX31740ATA+: FAQ
  • MAX31760AEE+: FAQ
  • +MAX31760AEE+T: FAQ
  • +MAX31785: FAQ
  • +MAX31785AETL+T: FAQ
  • MAX31790: FAQ
  • +MAX31790ATI+T: FAQ
  • +MAX31856MUD+: FAQ
  • +MAX32510: FAQ
  • +MAX32520/W+JU: FAQ
  • +MAX32520ATJJ/V+: FAQ
  • +MAX32550: FAQ
  • +MAX32552-LCJ+: FAQ
  • MAX32552: FAQ
  • +MAX32555/B+: FAQ
  • MAX32555: FAQ
  • +MAX32558: FAQ
  • +MAX32560: FAQ
  • +MAX32590-LNS+: FAQ
  • +MAX32620-EVKIT#: FAQ
  • +MAX32620-EVKIT: FAQ
  • +MAX32620FTHR#: FAQ
  • MAX32620FTHR: FAQ
  • +MAX32620ICQ+: FAQ
  • +MAX32620IWG+T: FAQ
  • +MAX32621-EVKIT#: FAQ
  • +MAX32621IWG+T: FAQ
  • +MAX32625-EVKIT#: FAQ
  • +MAX32625-EVKIT: FAQ
  • MAX32625: FAQ
  • +MAX32625ITK+: FAQ
  • +MAX32625MBED#: FAQ
  • +MAX32625MBED: FAQ
  • +MAX32625NEXPAQ: FAQ
  • +MAX32625PICO#: FAQ
  • +MAX32626-EVKIT#: FAQ
  • +MAX32626-EVKIT: FAQ
  • +MAX32626: FAQ
  • +MAX32630-EVKIT#: FAQ
  • +MAX32630FTHR#: FAQ
  • MAX32630FTHR: FAQ
  • +MAX32630ICQ+: FAQ
  • MAX32630IWG+: FAQ
  • +MAX32630IWG+T: FAQ
  • +MAX32631-EVKIT#: FAQ
  • MAX32631: FAQ
  • +MAX32631ICQ+: FAQ
  • +MAX32632: FAQ
  • +MAX32650-EVKIT#: FAQ
  • +MAX32650EVKIT: FAQ
  • +MAX32650GCE+: FAQ
  • +MAX32650GWQ+T: FAQ
  • MAX32651: FAQ
  • +MAX32651GCE+: FAQ
  • +MAX32652: FAQ
  • +MAX32655GWY+: FAQ
  • +MAX32660-EVKIT#: FAQ
  • +MAX32660-EVSYS#: FAQ
  • MAX32660: FAQ
  • +MAX32660EVKIT: FAQ
  • +MAX32660GTG+T: FAQ
  • +MAX32660GTGBL+: FAQ
  • +MAX32660GTGLA+T: FAQ
  • +MAX32660GWE+: FAQ
  • +MAX32665EVKIT#: FAQ
  • +MAX32665GXMBT+T: FAQ
  • +MAX32666FTHR#: FAQ
  • +MAX32666GWP+: FAQ
  • MAX32666GWPBT+: FAQ
  • +MAX32666GWPBT+T: FAQ
  • +MAX32668GWPBL+: FAQ
  • +MAX32670GTL+: FAQ
  • +MAX3421: FAQ
  • +MAX34440ETLA1+: FAQ
  • +MAX34446ETL+T: FAQ
  • +MAX34451ETNA1+: FAQ
  • +MAX34451ETNA2+: FAQ
  • +MAX34451ETNA3+: FAQ
  • +MAX34461AA00+: FAQ
  • +MAX34463EXQA3+: FAQ
  • +MAX3600: FAQ
  • +MAX3601GTL+: FAQ
  • +MAX3634: FAQ
  • +MAX3711: FAQ
  • +MAX3735AE/D: FAQ
  • +MAX3735AETG+: FAQ
  • +MAX3736ETE+: FAQ
  • +MAX3738: FAQ
  • +MAX3740AETG+: FAQ
  • MAX3740AETG: FAQ
  • +MAX3747AEUB+: FAQ
  • +MAX3748HETE+: FAQ
  • +MAX3761: FAQ
  • MAX3869EHJ+: FAQ
  • +MAX3869EHJ+T: FAQ
  • +MAX40056EVKIT#: FAQ
  • +MAX40200ANS+: FAQ
  • MAX40200AUK+: FAQ
  • +MAX40200AUK+T: FAQ
  • MAX40203ANS+: FAQ
  • +MAX40203ANS+T: FAQ
  • +MAX40213: FAQ
  • +MAX4137: FAQ
  • +MAX41460EVKIT: FAQ
  • +MAX41460GUB+: FAQ
  • +MAX41461GUB+T: FAQ
  • +MAX41463GUB+: FAQ
  • +MAX4201EUK+: FAQ
  • +MAX4207: FAQ
  • +MAX4222EEE+: FAQ
  • +MAX4311EEE+: FAQ
  • +MAX4370: FAQ
  • +MAX4383EEE+: FAQ
  • +MAX4427MJA/883B: FAQ
  • +MAX4428ESA+: FAQ
  • +MAX44299: FAQ
  • +MAX4444ESE/GG8: FAQ
  • +MAX4550EVKIT: FAQ
  • +MAX4820ETP+: FAQ
  • +MAX4821: FAQ
  • +MAX4896ATP+: FAQ
  • +MAX4915AELT+: FAQ
  • +MAX5048CAUT+: FAQ
  • +MAX5859EXW-D: FAQ
  • +MAX5902AAEUT+: FAQ
  • +MAX5903AAETT+: FAQ
  • +MAX5921FESA+: FAQ
  • +MAX5933AESA+: FAQ
  • +MAX5943AEEE+: FAQ
  • +MAX5947BESA: FAQ
  • +MAX5954AETX+: FAQ
  • +MAX5954LETX+: FAQ
  • +MAX5965A: FAQ
  • +MAX5969AETB+: FAQ
  • +MAX5969BETB+: FAQ
  • +MAX5969BEVKIT+: FAQ
  • +MAX5971AETI+: FAQ
  • +MAX5971BETI+: FAQ
  • +MAX5974AATE+T: FAQ
  • +MAX5974CETE+: FAQ
  • MAX5974D: FAQ
  • +MAX5974DATE+: FAQ
  • +MAX5974EETE+: FAQ
  • +MAX5977AETP+: FAQ
  • MAX5980: FAQ
  • +MAX5980AGTJ+: FAQ
  • +MAX5988A: FAQ
  • +MAX5991AETP+: FAQ
  • +MAX5995AATE+: FAQ
  • +MAX5995AETE+T: FAQ
  • +MAX5995BATE+: FAQ
  • +MAX5995CETE+: FAQ
  • +MAX6495: FAQ
  • +MAX6496ATA/V+: FAQ
  • +MAX6615AEE+: FAQ
  • +MAX6639FAEE: FAQ
  • +MAX6641: FAQ
  • +MAX6643LBBAEE+: FAQ
  • MAX6650: FAQ
  • +MAX6650EUB+: FAQ
  • +MAX6653AEE+: FAQ
  • +MAX6682MUA+T: FAQ
  • +MAX6684ESA+: FAQ
  • +MAX6816: FAQ
  • +MAX6839XSD2+: FAQ
  • +MAX6895AALT+: FAQ
  • +MAX6895AAZT/V+T: FAQ
  • +MAX7030HATJ+: FAQ
  • +MAX7032: FAQ
  • MAX7037: FAQ
  • +MAX7037EGL+T: FAQ
  • +MAX7037EVKIT#: FAQ
  • +MAX7461EUK+: FAQ
  • +MAX7474EAE+_T1: FAQ
  • +MAX77729XEWN+: FAQ
  • +MAX77823EWZ+: FAQ
  • +MAX77859AEWO+: FAQ
  • +MAX77932BEWO+: FAQ
  • +MAX77932EWO+T: FAQ
  • +MAX77972: FAQ
  • +MAX78000EXG+: FAQ
  • +MAX78000FTHR: FAQ
  • +MAX78700: FAQ
  • +MAX8535: FAQ
  • +MAX8790AETP+: FAQ
  • +MAX8804: FAQ
  • +MAX881: FAQ
  • +MAX8902: FAQ
  • +MAX8903: FAQ
  • +MAX9272: FAQ
  • +MAX9295AGTJ/V+: FAQ
  • +MAX9295EGTN/V+T: FAQ
  • +MAX9296AGTM/V+: FAQ
  • +MAX96716A: FAQ
  • +MAX96751: FAQ
  • +MAX96752: FAQ
  • +MAX96793: FAQ
  • +MAX98089ETN+: FAQ
  • +MAX98089EVKIT#WLP: FAQ
  • MAX98090: FAQ
  • +MAX98090AETL+T: FAQ
  • +MAX98090AEWJ+: FAQ
  • +MAX98090EVKIT#WLP: FAQ
  • +MAX98091: FAQ
  • +MAX98373: FAQ
  • +MAX9860ETG+: FAQ
  • MAX9867: FAQ
  • +MAX9867ETJ+: FAQ
  • +MAX9867EVKIT+: FAQ
  • MAX9880A: FAQ
  • +MAX9880AETM+: FAQ
  • +MAX9880AEVKIT#: FAQ
  • +MAX9947ETE+: FAQ
  • +MAXADCLITE+: FAQ
  • +MAXCOAX2STP-HSD#: FAQ
  • +MAXPOWERTOOL002#: FAQ
  • +MAXQ1741: FAQ
  • +MAXQ1743: FAQ
  • +MAXQ1744-DNS+: FAQ
  • +MAXQ617: FAQ
  • MAXQ7667: FAQ
  • +MAXQ7667AACM/V+: FAQ
  • +MAXQUSBJTAGOW-KIT#: FAQ
  • +MAXREFDES100#: FAQ
  • +MAXREFDES101 SOFTWARE FOR WINDOWS 10: FAQ
  • +MAXREFDES101#: FAQ
  • +MAXREFDES103#: FAQ
  • +MAXREFDES104#: FAQ
  • +MAXREFDES105#: FAQ
  • +MAXREFDES106: FAQ
  • +MAXREFDES117#: FAQ
  • +MAXREFDES132#: FAQ
  • +MAXREFDES145#: FAQ
  • +MAXREFDES150#: FAQ
  • +MAXREFDES16#: FAQ
  • +MAXREFDES165#: FAQ
  • +MAXREFDES212#: FAQ
  • +MAXREFDES220#: FAQ
  • +MAXREFDES280: FAQ
  • +MAXREFDES31#: FAQ
  • +MAXREFDES37#: FAQ
  • +MAXREFDES4#: FAQ
  • +MAXREFDES42#: FAQ
  • +MAXREFDES70#: FAQ
  • +MAXREFDES73#: FAQ
  • +MAXREFDES74#: FAQ
  • MAXREFDES74: FAQ
  • +MAXREFDES77#: FAQ
  • +MAXREFDES79#: FAQ
  • +MINIQUSB: FAQ
  • +NO PART NUMBER: FAQ
  • +NONE: FAQ
  • +OP07: FAQ
  • +OP27: FAQ
  • +OP37: FAQ
  • +OP90: FAQ
  • +PCB, MAX2850EVKIT+: FAQ
  • PD-1370: FAQ
  • +PD20-1-1210: FAQ
  • +PD28-3-1021-TMCL: FAQ
  • +PD42-1-1140-TMCL: FAQ
  • +PD42-1-1243-IOLINK: FAQ
  • +PD42-1-1370-TMCL: FAQ
  • +PD42-4-1370-TMCL: FAQ
  • +PD57-1-1076: FAQ
  • +PD57-1-1160-TMCL: FAQ
  • +PD57-1-1260-TMCL: FAQ
  • +PD57-1-1378-CANOPEN: FAQ
  • +PD57-2-1160-TMCL: FAQ
  • +PD60-3-1260-TMCL: FAQ
  • +PH-MODULES-TRINAMIC: FAQ
  • +QBL4208-100-04-025: FAQ
  • +QBL4208-41-04-006: FAQ
  • +QBL4208-61-04-013: FAQ
  • +QBL5704-116-04-042: FAQ
  • +QSH2818-32-07-006: FAQ
  • +QSH4218-41-10-035: FAQ
  • +REF02A: FAQ
  • +RS485: FAQ
  • +SC-USB-SPI: FAQ
  • +SSM2250: FAQ
  • +SSM2302: FAQ
  • +SSM2602: FAQ
  • +SSM2603: FAQ
  • +STM1E-SFP02: FAQ
  • +STM1E-SFP22: FAQ
  • +SW02: FAQ
  • +TEST: FAQ
  • +TMC USB-2-485: FAQ
  • +TMC2041-EVAL: FAQ
  • +TMC2041-LA: FAQ
  • +TMC2130-LA: FAQ
  • +TMC2208SILENTSTEPSTICK: FAQ
  • +TMC2209 SILENTSTEPSTICK: FAQ
  • +TMC2209-LA-T: FAQ
  • +TMC2226-BOB: FAQ
  • +TMC2240: FAQ
  • +TMC2590: FAQ
  • +TMC262C-LA: FAQ
  • +TMC2660C-PA-T: FAQ
  • TMC2660C-PA: FAQ
  • +TMC429-I: FAQ
  • +TMC4361A-LA: FAQ
  • +TMC457: FAQ
  • +TMC4671: FAQ
  • +TMC5031: FAQ
  • +TMC5041-LA: FAQ
  • +TMC5062-LA: FAQ
  • +TMC5072-LA: FAQ
  • +TMC5130-EVAL-KIT: FAQ
  • +TMC5130A-TA: FAQ
  • +TMC5160 SILENTSTEPSTICK: FAQ
  • +TMC5160-BOB: FAQ
  • +TMC5160-EVAL: FAQ
  • +TMC5160A-TA: FAQ
  • +TMC5240: FAQ
  • +TMC5272-EVAL-KIT: FAQ
  • +TMC6140-EVAL: FAQ
  • +TMC8462: FAQ
  • +TMCM-1043: FAQ
  • +TMCM-1070: FAQ
  • +TMCM-110-42-485: FAQ
  • +TMCM-1110 STEPROCKER: FAQ
  • +TMCM-1140-TMCL: FAQ
  • +TMCM-1160-TMCL: FAQ
  • +TMCM-1180-TMCL: FAQ
  • +TMCM-1240: FAQ
  • +TMCM-1260-CANOPEN: FAQ
  • +TMCM-1260-TMCL: FAQ
  • +TMCM-1270-CANOPEN: FAQ
  • +TMCM-1290: FAQ
  • +TMCM-142-IF-TMCL: FAQ
  • +TMCM-1630-2C: FAQ
  • +TMCM-1630-4U: FAQ
  • +TMCM-1633-CANOPEN: FAQ
  • +TMCM-1636-24V-CANOPEN: FAQ
  • +TMCM-1640: FAQ
  • +TMCM-1690: FAQ
  • +TMCM-310/SG: FAQ
  • +TMCM-3110-TMCL: FAQ
  • +TMCM-3212-TMCL: FAQ
  • +TMCM-3230-TMCL: FAQ
  • +TMCM-3314: FAQ
  • +TMCM-3351-TMCL: FAQ
  • +TMCM-6110: FAQ
  • +TMCM-6212-TMCL: FAQ
  • +TMCM-6214-CANOPEN: FAQ
  • +TMCM-6214-TMCL: FAQ
  • +TMCS: FAQ
  • +TRINAMIC MISC SERVICE: FAQ
  • +TRINAMIC PACKAGING SURCHARGE: FAQ
  • +USB-2-RTMI: FAQ
  • +USB2GPIO#: FAQ
  • +USB2PMB2#: FAQ
  • +VDSP-BLKFN-PC-FULL: FAQ
  • +VDSP-TS-PC-FULL: FAQ
  • +VISUALAUDIO: FAQ
  • +VT202: FAQ
  • +VT273SAFQ: FAQ
  • What does the "C01" denote in DS75S-C01+?
  • What should I do with unused I/O pins on the DS2482S?
  • +ZLP32300: FAQ
  • +_DS9093A: FAQ

What are the trade-offs between power consumption and conversion speed in the MAX1464?

Systems that operate with very low-power consumption benefit from the reduced ADC clock rate, FADC. Slower clock speeds require less operating current. Systems operating from a larger power consumption budget can use the highest FADC clock rate to improve speed performance over power performance. The ADC conversion times for various resolution and clock rate settings are summarized in the ADC Conversion Time table in the MAX1464 data sheet. The conversion time is calculated by the formula: TCONVERT = (number of FADC clocks per conversion) / FADC. The number of clocks per conversion is a function of the desired conversion resolution.
Tags: MAX1464 000095328 8052 Core Products Precision Microcontrollers